STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TOUCHGFX+STM32F0XX+TFT Display

Hello.I haven't found similar question. I am beginner with TOUCHGFX: Is it possible to use TOUCHGFX with STM32F0XX series with some cheap TFT Displays? As I read TOUCHGFX supports all of that drivers but I don't understand how to connect all componen...

CuAuPro by Associate II
  • 4080 Views
  • 6 replies
  • 0 kudos

Problem Using LTDC with USB in STM32H7

We are using stm32H743 We need a frame buffer of 150K to our LCD. we do not have an external RAM, so we use the 412K internal RAM.We also work with USB (Full speed mode).each peripheral work on it own , but not together. if we enable both of them the...

Hmizr.1 by Associate II
  • 1811 Views
  • 1 replies
  • 0 kudos

DCMI VSYNC not detected

I programmed DCMI interface, and I can see the VSYNC, HSYNC waveform on the pin of STM32L496, but no data are captured. I checked the register, found VSYNC_RIS is never be set to "1', looks like it does not detect signal change. I checked the regist...

0693W000000WXneQAG.jpg
hsong.11 by Associate II
  • 757 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.