2019-01-14 6:43 AM
Hello
i want to pass variable value from model to view.
Model has get function
uint8_t Model::getLanguage()
{
return (md_language);
}
Presenter also :
uint8_t LanguagePresenter::getLanguage()
{
return(model->getLanguage());
}
LanguageView::LanguageView()
{
selected_language = presenter->getLanguage();
}
when Presenter function is executed i have an exception : the model pointer is null.
If i put breakpoint i can see model object is created before presenter and view.
Why model pointer is null in prsenter function ?
I can we get data from model ?
thanks
regards
2019-01-15 12:28 AM
Hi @Professional,
The model pointer should definitely not be null. It is configured for the presenter whenever you transition to a new screen, automatically. Your approach seems correct. You should be able to get things from the model through the presenter, from the view.
Which compiler/project are you using? Is this an issue with both simulator and target project?
Thanks!
Best regards,
Martin
2019-01-15 12:41 AM
Hello
thanks for your reply
i' m using only simulator just for now (visual studio 2017 C++).
i've solved the problem by calling presenter->getLanguage(); from setupScreen() function instead of view constructor LanguageView::LanguageView()
best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.