2023-07-04 12:08 AM - edited 2023-07-04 12:10 AM
I am facing performance issues on several PC's I use to work with TouchGFX.
Time to start simulation for an example project (dice) is several minutes. A comparison with a private owned PC shows that the same project can be simulated in 27s, so I started to look for reasons of this performance issue.
In the known Issues section of the documentation is the following point listed:
LOGONSERVER environment variable
We have observed on a few computers that the TouchGFX is very slow (e.g. "Run simulator" does nothing for 30 seconds). It may help to set the environment variable LOGONSERVER to an empty value. In bash, the command is:
export LOGONSERVER=
Can someone tell me how to work with this environment variable on a windows PC? When I tried to check if this variable is available in CMD, I just get the information that no variable with that name exists
Solved! Go to Solution.
2023-07-13 2:15 AM
After some experiments we have found a solution for our performance issues.
For security reasons an application control software is used in our company. As TouchGFX was prohibited to be used with standard users, a priviledged admin user was used to run the software.
With that admin user we faced the performance issues.
After TouchGFX was added to a safe software list, we were able to run it with our normal users and the performance issues were gone.
2023-07-05 8:30 AM
Hello @VIKA ,
Which version of TouchGFX do you use? I know that we improved the proxy authentication management in TouchGFX 4.22.0 (see in the changelog), so that should be much more stable from 4.22.0. But if you are using it already, could you share your log file to us please? and we can start investigating it.
2023-07-05 11:53 PM
Hello @Osman SOYKURT
I am using version 4.22.0.
Attached you can find the output of the detailed log of TouchGFX when I start a simulation. If you need some additional data please let me know.
Best regards
Viktor
2023-07-10 2:01 AM
Hello @VIKA ,
Thanks for that, could you send me the TouchGFX Designer logs also, located at : "C:\Users\YOUR_USER_NAME\AppData\Roaming\TouchGFX-4.22.0\TouchGFXDesigner.log"
2023-07-10 3:00 AM
Hello @Osman SOYKURT ,
attached you can find the log file of two different PC's we are facing the performance issues. One has version 4.22.0 installed, the other one runs 4.21.4. The issues are similar.
2023-07-10 4:47 AM
Can you check what value you have for that variable on your machine?
In a Windows terminal, type "set" and look for LOGONSERVER variable.
2023-07-10 6:22 AM
This variable is set to a server in our company (connected via LAN)
I only got permission from the IT department to set it temporary to an empty value. Nevertheless I have seen no difference in performance.
I have attached the new log file but from what I can see it has not changed.
2023-07-13 2:15 AM
After some experiments we have found a solution for our performance issues.
For security reasons an application control software is used in our company. As TouchGFX was prohibited to be used with standard users, a priviledged admin user was used to run the software.
With that admin user we faced the performance issues.
After TouchGFX was added to a safe software list, we were able to run it with our normal users and the performance issues were gone.
2023-07-13 4:41 AM
Good to hear your issue is solved, and thanks for sharing it :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.