2019-04-09 2:48 AM
I'm trying to connect stm32f103c8t6 board with ILI9325 LCD display. I have created a driver for it in Atollic TrueStudio and run it successfully. Now, I am trying to transfer the driver to the Arduino IDE, because here it will be easier to integrate my code with the other code for this project. However, the driver doesn't work in Arduino IDE. The LCD is just blank.
I have tested the basic GPIO operation in Arduino IDE for stm32f1, it works fine. I have checked the pins on the LCD. They seem to receive command from the board. All the wiring is correct, because the screen works with the code from Atollic without any wiring change.
This is the driver code I use in Arduino IDE. It's basically the same as the one in Atollic. All I changed is the functions of initializing and setting GPIO.
#define LCD_RESET_Pin 9
#define LCD_CS_Pin 8
#define LCD_RS_Pin 7
#define LCD_WR_Pin 6
#define LCD_RD_Pin 5
#define TFT_W 320
#define TFT_H 240
#define WHITE 0xFFFF
#define BLACK 0x0000
#define BLUE 0x001F
#define RED 0xF800
#define MAGENTA 0xF81F
#define GREEN 0x07E0
#define CYAN 0x7FFF
#define YELLOW 0xFFE0
#define BROWN 0xBC40
#define BRRED 0xFC07 // brownish red
#define GRAY 0x8430 // gray
#define DARKBLUE 0x01CF // dark blue
#define LIGHTBLUE 0x7D7C // blue
#define GRAYBLUE 0x5458 // gray-blue
#define LIGHTGREEN 0x841F // light green
#define LIGHTGRAY 0xC618 // light gray
void write_cmd_tft(uint16_t command)
{
gpio_write_bit(GPIOA, LCD_RS_Pin, LOW);
gpio_write_bit(GPIOA, LCD_CS_Pin, LOW);
GPIOB->regs->ODR = command;
gpio_write_bit(GPIOA, LCD_WR_Pin, LOW);
delayMicroseconds(10);
gpio_write_bit(GPIOA, LCD_WR_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_CS_Pin, HIGH);
}
void write_data16_tft(uint16_t data)
{
gpio_write_bit(GPIOA, LCD_RS_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_CS_Pin, LOW);
GPIOB->regs->ODR = data;
gpio_write_bit(GPIOA, LCD_WR_Pin, LOW);
delayMicroseconds(10);
gpio_write_bit(GPIOA, LCD_WR_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_CS_Pin, HIGH);
}
#define cmd_write_ROM() write_cmd_tft(0x22)
#define cmd_write_pixel(color) write_data16_tft(color)
void write_reg_tft(uint16_t registerTFT, uint16_t dataTFT)
{
write_cmd_tft(registerTFT);
write_data16_tft(dataTFT);
}
void set_frame( uint16_t w1, uint16_t h1,
uint16_t w2, uint16_t h2)
{
if ((w1 >= TFT_W)||(h1 >= TFT_H)||(w2 >= TFT_W)||(h2 >= TFT_H));
write_reg_tft(0x50,h1);
write_reg_tft(0x51,h2);
write_reg_tft(0x52,w1);
write_reg_tft(0x53,w2);
write_reg_tft(0x20,h1);
write_reg_tft(0x21,w1);
}
void draw_pixel(uint16_t w, uint16_t h, uint16_t color)
{
write_reg_tft(0x20,h);
write_reg_tft(0x21,w);
write_reg_tft(0x22,color);
}
void draw_point(uint16_t w, uint16_t h,
uint8_t size,
uint16_t color)
{
uint16_t i = (uint16_t)size*size;
set_frame(w, h, w+size-1, h+size-1);
write_cmd_tft(0x22);
while(i--) write_data16_tft(color);
}
void fill_color (uint16_t color)
{
uint32_t i = (uint32_t)(TFT_W)*(TFT_H);
Serial2.print("Чи�?ло пик�?елей: ");
Serial2.println(i);
set_frame(0, 0, TFT_W-1, TFT_H-1);
write_cmd_tft(0x22);
while(i--) write_data16_tft(color);
}
void init_tft (void)
{
gpio_write_bit(GPIOA, LCD_RD_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_RESET_Pin, LOW);
delay(100);
gpio_write_bit(GPIOA, LCD_RESET_Pin, HIGH);
delay(100);
write_reg_tft(0x01,0x0000);
write_reg_tft(0x02,0x0700);
write_reg_tft(0x03,0x1038);
write_reg_tft(0x04,0x0000);
write_reg_tft(0x07,0x0000);
write_reg_tft(0x08,0x0302);
write_reg_tft(0x09,0x0000);
write_reg_tft(0x0A,0x0000);
write_reg_tft(0x0C,0x0000);
write_reg_tft(0x0D,0x0000);
write_reg_tft(0x0F,0x0000);
write_reg_tft(0x10,0x1290);
write_reg_tft(0x11,0x0007);
delay(100);
write_reg_tft(0x12,0x0092);
delay(100);
write_reg_tft(0x13,0x0E00);
delay(100);
write_reg_tft(0x29,0x0005);
write_reg_tft(0x2B,0x000E);
write_reg_tft(0x30,0x0004);
write_reg_tft(0x31,0x0307);
write_reg_tft(0x32,0x0002);
write_reg_tft(0x35,0x0206);
write_reg_tft(0x36,0x0A00);
write_reg_tft(0x37,0x0507);
write_reg_tft(0x38,0x0204);
write_reg_tft(0x39,0x0707);
write_reg_tft(0x3C,0x0405);
write_reg_tft(0x3D,0x0000);
write_reg_tft(0x50,0x0000);
write_reg_tft(0x51,0x00EF);
write_reg_tft(0x52,0x0000);
write_reg_tft(0x53,0x013F);
write_reg_tft(0x60,0xA700);
write_reg_tft(0x61,0x0001);
write_reg_tft(0x6A,0x0000);
write_reg_tft(0x80,0x0000);
write_reg_tft(0x81,0x0000);
write_reg_tft(0x82,0x0000);
write_reg_tft(0x83,0x0000);
write_reg_tft(0x84,0x0000);
write_reg_tft(0x85,0x0000);
write_reg_tft(0x90,0x0029);
write_reg_tft(0x92,0x0600);
write_reg_tft(0x93,0x0003);
write_reg_tft(0x95,0x0110);
write_reg_tft(0x97,0x0000);
write_reg_tft(0x98,0x0000);
write_reg_tft(0x07,0x0133);
fill_color(BLUE);
}
// the setup function runs once when you press reset or power the board
void setup() {
// initialize GPIO pins
pinMode(PA9, OUTPUT); //LCD_RESET_Pin
pinMode(PA8, OUTPUT); //LCD_CS_Pin
pinMode(PA7, OUTPUT); //LCD_RS_Pin
pinMode(PA6, OUTPUT); //LCD_WR_Pin
pinMode(PA5, OUTPUT); //LCD_RD_Pin
gpio_write_bit(GPIOA, LCD_RESET_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_CS_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_RS_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_WR_Pin, HIGH);
gpio_write_bit(GPIOA, LCD_RD_Pin, HIGH);
pinMode(PB15, OUTPUT);
pinMode(PB14, OUTPUT);
pinMode(PB13, OUTPUT);
pinMode(PB12, OUTPUT);
pinMode(PB11, OUTPUT);
pinMode(PB10, OUTPUT);
pinMode(PB9, OUTPUT);
pinMode(PB8, OUTPUT);
pinMode(PB7, OUTPUT);
pinMode(PB6, OUTPUT);
pinMode(PB5, OUTPUT);
pinMode(PB4, OUTPUT);
pinMode(PB3, OUTPUT);
pinMode(PB2, OUTPUT);
pinMode(PB1, OUTPUT);
pinMode(PB0, OUTPUT);
init_tft();
}
// the loop function runs over and over again forever
void loop() {
}What it's supposed to do is to initialize the LCD and to fill it in blue. Instead, it's just a blank screen.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.