2025-07-03 6:12 AM - edited 2025-07-03 6:13 AM
Hello,
I use a STM32F103 MCU and I use the RBIT instruction (as an CMSIS inline functinon). The instruction works properly and I can see the rbit instruction in the disassembly window (for this project I have to use an old TrueSTUDIO IDE).
According to the ARM documentation this MCU could not execute the RBIT instruction because it is a Cortex-M3 r1p1 core (CPUID: 0x411fc231) which does not have this instruction. In spite of this the instruction seemly works and the "PM0056 Programming manual" (STM32F10xxx/20xxx/21xxx/L1xxxx) mentions too the instruction without making any difference about the revisions.
Can someone help clear up this confusion?
Solved! Go to Solution.
2025-07-03 6:36 AM
Most "STM32F103" chips are counterfeit. Is this one of them?
Can you link to documentation saying RBIT is not supported? I could not find it.
2025-07-03 6:36 AM
Most "STM32F103" chips are counterfeit. Is this one of them?
Can you link to documentation saying RBIT is not supported? I could not find it.
2025-07-03 8:03 AM
> Can you link to documentation saying RBIT is not supported? I could not find it.
Yes, I misguided myself about the documentation, after checking it again, the RBIT is indeed part of the Cortex-M3 instruction set, independetly form the chip revision. The STM32F103 is surely genuine because it comes from a big and reliable distributor.
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.