2020-02-11 2:30 AM
I have designed my small component as a custom wedget that will be embeded in many screens. This component need do some data interations with background system.
As document suggested, I would like to use MVP architecture to implement data exchanges. But I find that the presenter is at screen level, not the wedget level. So I have to re-transfer data through screen/view to it's internal componet? And I have to do it in every screen that used the component.
Can I do data exchanges at component level with MVP concept?
2020-02-11 12:31 PM
"Because TouchGFX is implemented in C++ you have the option of taking advantage of object-oriented paradigms in your screens. If for instance all your screens need to display a status bar at the top, showing current time, battery level, et cetera you can create a base view class containing the status bar only and have all your views deriving from this class, so you get the status bar functionality automatically."
Source: https://touchgfx.zendesk.com/hc/en-us/articles/205717801-The-Screen-Concept-and-Model-View-Presenter
2020-02-11 6:48 PM
Thank for your reply and I understand your method, it applies on small project only.
After I checked along the current data exchange path, I implemented another way, maybe helpful for someone else, that is.
For any comonent that need data interaction, it register a callback function onto the model when created and un-register it before destroy, model will call all the callbacks at tick event.
So every component can be more indepedent each other.
2022-10-24 3:11 AM
Is there an updated link to this ressource?
2022-10-24 6:34 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.