2020-10-04 9:42 AM
I am having 10.1 Inch display with CTP. The touch controller is ILI2511 at USB interface only. It is configured as multi touch point touch pad.
I connected touch panel with PC, it is detected by PC and multi touch test screen appears on PC screen, where I can see touch point where I touches the touch panel.
I want to use this panel with STM32H7 MCU at USB interface. Can anyone help.
2020-10-04 9:43 PM
Hello,
We do not have examples with USB interface touch controller.
However the principle is simple. In STM32TouchController.cpp file situated in TouchGFX/target/ folder, you initialize your touch controller driver (see void STM32TouchController::init()) and then in bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y) you retrieve the coordinates from your TouchController. You can look at any Application Template available in TouchGFX Designer that has a touchable screen for reference. Note that you need to have a working driver in order to make things possible. Also TouchGFX do not support multi touch so you will only be able to pass one point coordinates at a time to the framework.
/Alexandre
2023-11-18 5:10 AM
hello
could you finally drive it?I have the same problem and I need help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.