2026-04-02 6:50 AM - last edited on 2026-04-08 2:35 AM by Amel NASRI
Hello @INaee.1 ,
I am working with the STM32H743BIT6 using the LTDC peripheral to drive an RGB display.
The display I am using does not have HSYNC and VSYNC signals and operates only in DE (Data Enable) mode. I have attached the display datasheet and pin connection for reference.
Based on the datasheet timing specifications, I configured the LTDC parameters accordingly. Since the display does not use HSYNC and VSYNC, I configured them as constant high signals (logic 1) and set the rest of the LTDC timing parameters as specified.
However, the display is not showing any image. The backlight turns on, but the screen remains black.
Below are the key points of my configuration:
I would like to know:
Edit: moved from How setup LTDC to DE MODE.
2026-04-03 12:17 AM
Hi Anil ...
is your problem solved ?
if not , then send me MX project file and I will configure it for you.
for that I also need schematic of your board.
I have lot of experience with TouchGFx ..
Here is my latest experiment with Google Nexus 7 , 1280x800 TFT with stm32h745 board.
Here is my dev board with stm32h745
regards
Imran
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.