2026-01-13 12:55 PM
Touchgfx 4.26.0 (and was same on 4.24.0) keyboard examples are the same resolution although there are (3) resolution of display resolution selections
They all display the keyboard size as approx. measured 43 mm (1.7 inches) X 33mm (1.3 inches) on a 5-inch display 800 X 480 resolution. To be usable we believe the keyboard needs to be about 1.5 to 2 times larger than present. (about 25% LARGER) See details in pdf attachment
Solved! Go to Solution.
2026-01-19 2:39 AM
Hello @JD_Jenzano ,
Indeed, the keyboard example is just to showcase how to realize a keyboard, you can copy or get inspiration from it to realize your own keyboard. I believe there is also some other keyboards shared by our community members that are accessible here :
2026-01-19 2:39 AM
Hello @JD_Jenzano ,
Indeed, the keyboard example is just to showcase how to realize a keyboard, you can copy or get inspiration from it to realize your own keyboard. I believe there is also some other keyboards shared by our community members that are accessible here :
2026-02-03 1:01 PM
Osman SOYKURT – I just got back to this topic –
I only posted my comment so that others could gain some insight to my experience with the keyboard example. I never really thought I would get response. Thank you for your information and the inspiration! – We have been using the keyboard example and really have found it useful – We were aided using a video from ControllersTech -Touch GFX #7. How to Implement Keyboard Tutorial. If you want to help us and others you could outline the best steps you suggest getting the keyboard larger. I currently do not know how to do that but I am sure I can figure it out later. It is helpful to have some keyboard and keypad examples in TouchGFX it helps getting to the focused needs of the project functionality requirements quickly. Even though we understand we are likely going to need to build the actual to fit our actual needs. To help optimize our time we also use the Keypad Custom Widget.zip from the links you responded with by Juliette CRESPO ST Employee – That example size (and example functionality) on the screen works well and is very close to what we will need. Our focus goal is to get to the Hardware most effectively ASAP. Saving time on software widgets greatly help along the path and it helps assure the hardware will be sufficient before it is implemented! Again, thank you for your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.