2021-01-12 5:28 AM
I have problem with the DCMI in STM32H7A3.DCMI FIFO never get filled and the DMA interrupt never start. does any one faced this issue with this new uc?
I have Camera system runs on STM32H743 and now we use the new STM32H7A3 but the problem the DCMI FIFO never get filled so the DMA never start the transfer. i have the Vsync and H sync working and the pixel clock too. I wonder if there is informations related to this new uc.
Solved! Go to Solution.
2021-01-14 7:42 PM
Problem solved. Its bug in the Cube IDE. It does not generate the function to link the DCMI with the DMA. I speak about the HAL Link DMA function
2021-01-14 7:42 PM
Problem solved. Its bug in the Cube IDE. It does not generate the function to link the DCMI with the DMA. I speak about the HAL Link DMA function
2021-01-15 4:00 AM
Hi @Community member ,
Thanks for sharing the solution to the issue you faced.
In order to fix it permanently at STM32CubeIDE (and STM32CubeMX) sides, could you please precise the used version of these tools? Are you aligned with last revisions?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-01-17 11:44 PM
Hi @Amel NASRI
Cube IDE version 1.5.1
Mahmoud
2021-01-18 7:13 AM
Hi @Community member ,
The problem is confirmed, I reported it internally and our STM32CubeMX team will take care to fix it in next releases.
Thanks,
Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-04-06 2:17 AM
Hi @Community member ,
I am pleased to inform you that the issue was fixed in the latest STM32CubeMX and STM32CubeIDE versions.
Please try them, and keep me informed if there is any faced issue.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-04-22 2:28 AM
@Amel NASRI
Hi ,
Thank you.
I only have one question and i hope you can help with it
Can the DMA2D in the H7 reconfigured to accept the YCBCR from the DCMI so it can convert to RGB565 or way to organize the YCBCR from the DCMI into 8x8 MCU as it expected from the hardware jpeg decoder?
Mahmoud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.