STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Issue to use DCMI with STM32H7A3 (DMA mode)

I have problem with the DCMI in STM32H7A3.DCMI FIFO never get filled and the DMA interrupt never start. does any one faced this issue with this new uc?I have Camera system runs on STM32H743 and now we use the new STM32H7A3 but the problem the DCMI FI...

MSale.1 by Senior
  • 1522 Views
  • 6 replies
  • 0 kudos

Resolved! STM32 processor with LTDC and 800x480 resolution

I am new to touchgfx ide and also LCD interface. i am planning to use STM32 with LTDC interface for interfacing TFT lcd. But i am a little confused while selecting the development board. I want to use a screen with a resolution of 800x480. but i can ...

SS.Sagar by Associate III
  • 2172 Views
  • 1 replies
  • 0 kudos

Resolved! Location Type fatal error: -texts/TypedTextDatabase.hpp: No such file or directory -touchgfx/Bitmap.hpp: No such file or directory -touchgfx/hal/HAL.hpp: No such file or directory

These errors arise at my first attempt to compile the generated code from the ioc file before coding any task functions. This is just to check everything is setup correctly before delving into code. Please note this is my first touchGFX app.

ksale.1 by Senior II
  • 4293 Views
  • 5 replies
  • 0 kudos

SwipeContainer Pages use too much .bss memory

Hello,We have almost finished a product using touchgfx. We have 512k internal RAM on our stm32f767.Based on profiling the linker file, 360k of our program .bss goes into internal RAM. Of that 360k .bss, a staggering 320k is only from SwipeContainer p...

VSimu.1 by Associate III
  • 3746 Views
  • 9 replies
  • 0 kudos

How to create a project without an RTOS?

I have a STM32H7B3I-DK, and I can create a TouchGFX project with FreeRTOS and it works great.I wanted to research not using an RTOS, so using CubeMX I created a project based on the STM32H7B3I-DK, which includes TouchGFX, but does not have an RTOS. T...

hwsw by Associate II
  • 1926 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.