2023-05-12 8:54 AM
2023-05-12 9:01 AM
STM32U599
https://www.st.com/en/microcontrollers-microprocessors/stm32u599-5a9.html
2023-05-12 9:04 AM
Thank you for the support, is their a 48pin package avaliable
2023-05-12 9:10 AM
or does using this fuctionality require memorey exctra
2023-05-12 9:42 AM
Graphics tend to require a lot of memory and pins. The resolution of the display being a primary driver. Enumerate your wish list of features for a display, it will probably help narrow down what's actually appropriate.
According to the cited page, 100 pins and upward
I don't think it uses DSI.
If your needs are less exotic you can attach self-contained screens to pretty much any MCU. Some of the 320x240 displays have on-board memory, and interface via an SPI connection.
2023-05-15 12:51 AM
If i attacch the display to this MCU STM32U535CC - Ultra-low-power with FPU Arm Cortex-M33 MCU with TrustZone, 160 MHz with 256 Kbytes of Flash memory - STMicroelectronics it should have enough memorey to support the appliaction
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.