2016-03-09 7:37 AM
Hello,
Recently I got the STM32L476 Nucleo-64 board. Now I am trying to interface it with LCD display.#define Bit_SET GPIO_PIN_SET
#define Bit_RESET GPIO_PIN_RESET
void LCD_WriteNibble(unsigned char nibbleToWrite)
{
int delayCnt;
HAL_GPIO_WritePin(LCD_Ctrl_Port, LCD_EN_Pin, Bit_RESET);
for(delayCnt=0; delayCnt<5000; delayCnt++);
HAL_GPIO_WritePin(LCD_Data_Port, LCD_D4_Pin, (nibbleToWrite & (unsigned char)0x01));
HAL_GPIO_WritePin(LCD_Data_Port, LCD_D5_Pin, (nibbleToWrite & (unsigned char)0x02));
HAL_GPIO_WritePin(LCD_Data_Port, LCD_D6_Pin, (nibbleToWrite & (unsigned char)0x04));
HAL_GPIO_WritePin(LCD_Data_Port, LCD_D7_Pin, (nibbleToWrite & (unsigned char)0x08));
HAL_GPIO_WritePin(LCD_Ctrl_Port, LCD_EN_Pin, Bit_SET);
for(delayCnt=0; delayCnt<5000; delayCnt++);
HAL_GPIO_WritePin(LCD_Ctrl_Port, LCD_EN_Pin, Bit_RESET);
}
void LCD_Init2()
{
int i=0, delayCnt=0;
for (delayCnt=0;delayCnt<1000000;delayCnt++);
GPIO_ResetBits(GPIOA, LCD_RS_Pin | LCD_EN_Pin | LCD_RW_Pin);
for(i = 0; i < 3; i++) {
LCD_WriteNibble(0x03);
for(delayCnt = 0; delayCnt < 1000000; delayCnt++);
}
LCD_WriteNibble(0x02);
for(delayCnt = 0; delayCnt < 600000; delayCnt++);
LCD_WriteNibble(0x02);
for(delayCnt = 0; delayCnt < 600000; delayCnt++);
LCD_WriteNibble(0x02);
LCD_WriteNibble(0x08);
for(delayCnt = 0; delayCnt < 600000; delayCnt++);
LCD_WriteNibble(0x00);
LCD_WriteNibble(0x08);
for(delayCnt = 0; delayCnt < 600000; delayCnt++);
LCD_WriteNibble(0x00);
LCD_WriteNibble(0x01);
for(delayCnt = 0; delayCnt < 600000; delayCnt++);
LCD_WriteNibble(0x00);
LCD_WriteNibble(0x06);
for(delayCnt = 0; delayCnt < 600000; delayCnt++);
LCD_WriteNibble(0x00);
LCD_WriteNibble(0x0C);
for(delayCnt = 0; delayCnt < 600000; delayCnt++);
}
Unfortunately, it isn't working and I can't figure out why. There is still a bunch of rectangles in upper row:
2018-07-30 2:38 AM
2018-07-30 5:42 AM
Yes, the larger posts seem to have an issue, you'll need to talk to @brk about transition efforts/schedules.
Here the Format Code Block data is damaged too.
I would however generally advise against posting answers to threads which are several years old, the OP is unlikely to find the answer or be alerted.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.