2022-03-03 3:57 AM
Hi,
At this stage I have tried everything but the LCD is not showing any graphics.
I have created the project in the STMCubeIDE and configured the LTDC & frame buffer parameters as shown in the pics.
I have also added the fmc initialization code in the main loop.
Could anyone kindly direct me in the right direction? Really thanks
2022-03-03 4:00 AM
2022-03-03 9:55 AM
Start LTDC only , no FMC, no Touchgfx
Layer 0 Framebuffer place into internal RAM .
2022-03-03 10:02 AM
Check obvious things like pins and clocks. Both at a basic configuration level, and that for example the clocking of the display is occurring. Back-light powered, etc.
Assume no one here is familiar with the specifics of your board, or the STM32 part you're using.
2022-03-04 12:11 AM
Thanks for your feedback and I apologize for not providing info regarding the controller, currently, I'm testing the LCD on STM32F429I-DISC1 by removing its onboard LCD.
Turned out the LCD which I was using for somehow not displaying any data (only backlight was working as I was providing power externally to it) and when I changed to another LCD it started displaying blue color while in touchGFX it was red. and If I add any text or button it just shows some random colour.
My question is, this garbage colour is it because of a wrongly configured frame buffer or something else?
One more thing I encountered is all of a sudden compiler is giving an error for region flash overflowed, while there's only one screen on it and nothing else.
Really appreciate any feedback.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.