2022-09-08 10:35 PM
2022-09-12 5:37 AM
libraries not visible to the project, check lib paths and where it is trying to fetch them from, and if they are there.
Create a new project, have that build successfully, and review how that's constructed.
2022-09-12 12:29 AM
Hello @Roger.ch ,
Did you already try to uninstall and reinstall TouchGFX ?
Otherwise, please also follow the introduction guidelines. There is maybe something in the installation procedure which might help you solve your issue.
Thanks,
/Yoann
2022-09-12 12:43 AM
good luck @Roger.ch , it looks like your colleage left some barbed wire behind for the next guy
2022-09-12 1:14 AM
Hi Yoann.
Thank you for your submission.
I have uninstalled versions 4.18 and 4.20 and reinstalled very strictly according to instructions.
Unfortunately without much success.
Where should this "module" be installed and where are the entries so that the ID.exe can find them?
Greetings, Roger
2022-09-12 4:50 AM
Can you share your project here please ?
/Yoann
2022-09-12 5:37 AM
libraries not visible to the project, check lib paths and where it is trying to fetch them from, and if they are there.
Create a new project, have that build successfully, and review how that's constructed.
2022-09-12 6:15 AM
Thank you very much for your comment. The project is now running.
Sometimes you can't see the forest for the trees.
When comparing a new project I noticed that the directory ".....\Project\Middlewares\ST\TouchGFX\touchgfx\lib\core\cortex_m7\gcc" was extremely empty.
I then simply copied the folder from a self-generated custom project. And what can I say, it works.
Many thanks to all involved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.