STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

BUG on TouchGFX4.20.0

Hi,I think ther is a bug on touchGFX 4.20.0If you choose the object "static graph"Insert in "Y-axis Range Min" = 60Insert in "X-axis Range Min" = 0Insert in "X-axis Range Max" = 8Then click into the box Y-axis Min (where you have insert 60), now the ...

MDi D.1 by Associate II
  • 724 Views
  • 0 replies
  • 0 kudos

I would like to use "setValueSetAction" and/or "setValueUpdatedAction" on the Progress Bar, but I couldn't figure out the callback generation.

I'm trying to generate a callback for tracking the progress bar updates. For this purpose I would like to use "setValueUpdatedAction" or "setValueSetAction" functions (which are defined in library). However I couldn't generate the callback or handler...

JJGok by Associate II
  • 2445 Views
  • 4 replies
  • 0 kudos

Moving the slider Knob without Touch.

Hi...I have configure the slider Widget using TOUCHGFX & it is working fine with Touch. But the want to Configure the slider without touch i.e., When I give some Data through Usart , according to that data the slider knob has to move (Without touchin...

PM.5 by Associate III
  • 1992 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.