2023-02-11 2:39 AM
I'm trying to get my 4.16.1 project updated to 4.21.1, but the conversion fails. I then tried installing all the versions in between, and can see that it fails from 4.18.1 to 4.19.0:
The full error message:
C:/TouchGFX/4.19.0/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems/version.rb:214:in `initialize': Malformed version number string - (ArgumentError)
from C:/TouchGFX/4.19.0/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems/version.rb:205:in `new'
from C:/TouchGFX/4.19.0/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems/version.rb:205:in `new'
from C:/touchgfx/4.19.0/touchgfx/framework/tools/textconvert/upgrader.rb:42:in `<class:Main>'
from C:/touchgfx/4.19.0/touchgfx/framework/tools/textconvert/upgrader.rb:25:in `<main>'
2023-02-13 12:47 AM
Hello @KKark,
Could you please share your project, so we could try to reproduce the issue ?
Thanks,
/Yoann
2023-02-22 2:51 AM
I also see the same error when upgrading from my V4.10 project
The zipped project is 89MB if you wish me to send this to you.
2023-02-23 6:06 AM
Hello,
You can send us your .touchgfx file only, should be sufficient for us to open the project at least.
/Osman
2023-02-23 6:20 AM
2023-02-27 2:55 AM
Hello brianshankland9,
Sorry but no attached file is visible, could you retry to upload it? (you can send it to me or @Yoann KLEIN in PM if you prefer)
/Osman
2023-03-02 3:58 AM
2023-03-07 2:16 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.