2021-07-10 1:28 AM
185/5000
Win10 system using the CLion IDE, in the compilation environment of WinGW, using Cmake and arm-none-eabi-gcc toolchain compilation connection static library stemwin532_cm4_os_gcc. a,
CMake Error at CMakeLists.txt:68 (target_link_libraries):
"Cannot specify link libraries for target "demo" which is not built by this project."
mingw32-make.exe: *** [cmake_check_build_system] Error 1
2021-07-10 1:31 AM
my Cmakelist
This file is generated by STM32CubeMX.
link_directories(STemwin/Include)
link_libraries(STemwin/GUI_Lib)
add_executable(${PROJECT_NAME}.elf ${SOURCES} ${LINKER_SCRIPT})
target_link_libraries(${PROJECT_NAME} STemWin532_CM4_OS_GCC.a)
Is the library available only under Linux?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.