2022-11-20 1:32 AM
2022-11-22 4:36 AM
Hello @MDesh.2,
Let me first welcome you to the STM32 Community :)
The demonstration software supporting the X-NUCLEO-GFX01M1 expansion boards is available from the X-CUBE-DISPLAY Package offering the needed drivers as well as simple examples.
You can review and port the application from STM32L4 available in the package:
X-CUBE-DISPLAY-Vx.x\Projects\NUCLEO-L476RG\Applications\
Have a look at this manual for configuration with NUCLEO-F411RE board:
UM2750 SPI display expansion boards for STM32 Nucleo-64 - User manual
You can also open TouchGFX Designer and import the code from STM32G0 Board. Make sure to modify the the pins.
Imen
2022-11-22 6:36 AM
Thank you very much!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.