2026-03-11 11:46 AM
Setup: STM32F411RE + STM32CubeIDE + X-CUBE-AZRTOS-F4 v1.1.0 + TIM4 as HAL
timebase Problem: Thread runs once, toggles LED, then hangs inside tx_thread_sleep(50) and never wakes up. Debugger shows:
System Timer thread → State: SUSPENDED, Run Count: 0
Thread 1 → State: SLEEP, Run Count: 1 System Timer never runs, so sleeping threads never wake up.
Question: Why is the System Timer thread never getting scheduled? Any known issues with X-CUBE-AZRTOS-F4 v1.1.0?
2026-03-17 6:31 AM
Hello @SAID_embadded ,
The symptoms you see suggest that SysTick cannot preempt your thread, so the ThreadX timer interrupt never runs.
This often happens when the NVIC priority configuration is not compatible with the ThreadX port.
To confirm, could you please tell us:
Kind regards,
DHIF Khaled
2026-03-18 8:07 AM
yes it realy work when i add this ligne : HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
befor MX_ThreadX_Init();
it really work but why??
in addition when i installed the middleware AZURE and igenerate the code the cube MX it didn't generate this MX_ThreadX_Init(); by default i add it manually by my self but it shall be declared by default i dont know why it not declared by default
2026-03-23 8:15 AM
Hello @SAID_embadded ,
In the ThreadX low‑level startup, the following assembly configures SysTick, SVC, and PendSV priorities directly:
/* Configure handler priorities. */
LDR r1, =0xFF000000 @ SVCl, Rsrv, Rsrv, Rsrv
STR r1, [r0, #0xD1C] @ SHPR2: SVC = 0xFF (lowest)
LDR r1, =0x40FF0000 @ SysT, PnSV, Rsrv, DbgM
STR r1, [r0, #0xD20] @ SHPR3: SysTick = 0x40, PendSV = 0xFF
On STM32F4 (4 priority bits) this means SysTick has pre‑empt priority 4, while SVC and PendSV are at 15 (lowest). This setup assumes a grouping with pre‑emption bits (e.g. NVIC_PRIORITYGROUP_4), so SysTick can preempt threads and PendSV stays the lowest for context switching. If you switch to 0 pre‑emption / 4 subpriority, these assumptions break, and the System Timer thread may never run, causing tx_thread_sleep() to never wake up.
Regarding your second point, that's most likely an issue from the code generation by CubeMX, this will be reported internally so it can be addressed in a future update of the X‑CUBE‑AZRTOS / CubeMX integration.
Kind regards,
DHIF Khaled
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.