2018-05-18 7:38 PM
I am using the stm32f769 - eval board.
And, I am using the DSI to HDMI adapter.
I am trying to use the ADV7533 to 1024x768 , 16bit on B-LCDAD-HDMI1.
However, I do not know how to set adv7533.
I did a search but there is no related information or documentation.
Do you know how to set parameters?or,
Can you tell me the parameter value?I do not know what the MCU used in the following, but it is the data I searched on the internet.
/_________________________________________________________________________________
/*adv7533*/
46 { 640, 480, 96, 2, 48, 16, 33, 10, 25170000, 60},/*640x480p -1*/ 47 { 720, 480, 62, 6, 60, 19, 30, 9, 27000000, 60},/*720x480p -2*/ 48 { 720, 480, 62, 6, 60, 19, 30, 9, 27000000, 60},/*720x480p -3*/ 49 {1280, 720, 40, 5, 220, 110, 20, 5, 74170000, 60},/*1280x720p -4*/ 50 {1980, 1080, 44, 5, 148, 88, 15, 2, 74170000, 60},/*1980x1080i -5*/ 51 { 720, 480, 62, 3, 114, 17, 15, 5, 27000000, 60},/*720x480p -6*/ 52 { 720, 480, 62, 3, 114, 17, 15, 5, 27000000, 60},/*720x480p -7*/ 53 {1440, 240, 124, 3, 114, 38, 15, 4, 27000000, 60},/*1440x240p -8*/ 54 {1440, 240, 124, 3, 114, 38, 15, 4, 27000000, 60},/*1440x240p -9*/ 55 {2880, 480, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x480i -10*/ 56 {2880, 480, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x480i -11*/ 57 {2880, 240, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x240p -12*/ 58 {2880, 240, 248, 3, 228, 76, 15, 4, 54000000, 60},/*2880x240p -13*/ 59 {1440, 480, 124, 6, 120, 32, 30, 9, 54000000, 60},/*1440x480p -14*/ 60 {1440, 480, 124, 6, 120, 32, 30, 9, 54000000, 60},/*1440x480p -15*/ 61 {1920, 1080, 44, 5, 148, 88, 36, 4, 148350000, 60},/*1920x1080p -16*/ 62 { 720, 576, 64, 5, 68, 12, 39, 5, 27000000, 50},/*720x576p -17*/ 63 { 720, 576, 64, 5, 68, 12, 39, 5, 27000000, 50},/*720x576p -18*/ 64 {1280, 720, 40, 5, 220, 440, 20, 5, 74170000, 50},/*1280x720p -19*/________________________________________________________________________________/
However, from the performance of DSI, I know that 1024x768 is the best.
I want to set 1024x768, 16bit, RGB565, 2lane .....Thank you for knowing how to set parameters.It's difficult ... Hue..ã… ã…
2018-05-18 9:08 PM
I think you run out of bandwidth, the maximum pixel clock is 62.50 MHz for 16-bit and 41.67 MHz for 24-bit
I modified stm32f769i_discovery_lcd.c the parameters are ordered differently, and you have to program the LTDC and PLLs too.
{1024,136,160, 24, 768, 6, 29, 3, HDMI_ASPECT_RATIO_4_3, LCD_DSI_PIXEL_DATA_FMT_RBG565}, // 1024x768 62.50 MHz 16-bit
// Acer reports as 1024x768 H:46KHz V:57Hz2018-05-19 2:25 AM
did you consider SPI LCD ?
is your image active ?
can you send a link to the Ap note on the
adv7533
?2018-05-19 8:20 AM
https://community.st.com/0D50X00009XkW5nSAF
http://www.analog.com/media/en/technical-documentation/application-notes/AN-1pdf
2018-05-21 5:55 PM
Thank you for your help.
LCD wants to use PC Monitor.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.