2019-04-30 6:32 AM
I am trying to use STM32CubeIDE for with STM32F429i DISC1 for generating code with TouchGFX enabled in Device configuration tool. I have configured Touchgfx options as shown below.
After clicking EXECUTE button in touchgfx tab, touchgfx window opens.
In touchgfx, while trying to Generate code I am getting error. I have attached output_PostGenerate.log file
After closing TouchGFX, when i am trying to build project i am getting following errors.
18:48:16 **** Incremental Build of configuration Debug for project T2 ****
make -j4 all
arm-none-eabi-gcc "../Src/stm32f4xx_it.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DDEBUG -DSTM32F429xx -c -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../TouchGFX/gui/include -I../TouchGFX/generated/fonts/include -I../Drivers/BSP/Components/exc7200 -I../Drivers/BSP/Components/ts3510 -I../Drivers/BSP/Components/stmpe811 -I../Drivers/STM32F4xx_HAL_Driver/Inc -I../TouchGFX/generated/texts/include -I../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../Src -I../TouchGFX/generated/images/include -I../Drivers/BSP/Components/ili9341 -I../Drivers/STM32F4xx_HAL_Driver/Inc/Legacy -I../Middlewares/ST/STM32_USB_Host_Library/Core/Inc -I../Middlewares/ST/STM32_USB_Host_Library/Class/CDC/Inc -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../Inc -I../Drivers/CMSIS/Include -I../Middlewares/ST/TouchGFX/touchgfx/framework/include -I../TouchGFX/generated/gui_generated/include -I../Drivers/BSP/Components/Common -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Drivers/BSP/Components/ampire480272 -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Src/stm32f4xx_it.d" -MT"Src/stm32f4xx_it.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Src/stm32f4xx_it.o"
arm-none-eabi-gcc -o "T2.elf" @"objects.list" -mcpu=cortex-m4 -T"C:\work\T2\STM32F429ZITX_FLASH.ld" --specs=nosys.specs -Wl,-Map="T2.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
Startup/startup_stm32f429zitx.o: In function `LoopFillZerobss':
C:/work/T2/Debug/../Startup/startup_stm32f429zitx.s:113: undefined reference to `main'
Src/stm32f4xx_it.o: In function `LTDC_IRQHandler':
C:/work/T2/Debug/../Src/stm32f4xx_it.c:205: undefined reference to `hltdc'
Src/stm32f4xx_it.o: In function `DMA2D_IRQHandler':
C:/work/T2/Debug/../Src/stm32f4xx_it.c:219: undefined reference to `hdma2d'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:51: T2.elf] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
18:48:20 Build Failed. 4 errors, 0 warnings. (took 3s.477ms)
2019-05-07 12:41 AM
Hi guys,
Thanks for pinging me @Mon2. As you've no doubt realized, @njinodra, there are some quirks. The best thing i can do is pass it on right now, but we could always try to fix your compiler errors together, but clearly the project isn't being generated correctly (undefined references). Even if we do fix the compiler errors, there may be underlying problems.
Let me know what you want to do.
/Martin
2019-05-07 1:34 AM
@njinodra, could you please share your project with me?
I just helped someone else getting their CubeIDE project to compile. I found the following two issues that might also be helpful to know about:
If you share your project i will take a look.
Best regards,
Martin
2019-05-07 3:43 AM
@njinodra,
I have a suspicion that you've selected "C" as the project when you started it (Default). This is incompatible with a "Touchgfx" project which is C++.
The three symbols that are undefined come from BoardConfiguration.cpp and i'm preeetty sure that these aren't getting compiled.
2019-05-08 12:29 AM
I guess this is one of the "caveats" of an Eclipse based solution. You're most likely using a lot of standard components, but what you'd really want is a way to create a "TouchGFX" project which is then, implicitly, is a C++ project.
Maybe there'll be more cases like this, but it's definitely something we can talk to the CubeIDE team about. It's great to have this kind of real life usage information.
Best regards,
Martin
2019-05-08 1:19 AM
When a new project is created in the embedded CubeMX, on the first page either C or C++ can be selected (page where the project name is typed in).
2019-05-21 4:28 AM
Check out the new sticky on TouchGFX/CubeIDE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.