2020-02-07 12:00 AM
I need to measure memory usage in my TouchGFX application. Is there a way to do this?
2020-02-07 12:39 AM
First starting point would be the map file generated by the linker.
Not sure if the TouchGfx vendor supplies some additional evaluation tool for gfx-internal memory consumption.
2020-02-07 2:44 AM
Another approach would be starting a project in new version CubeMX 5.5 and enabling all necessary peripherals for touchgfx (ltdc, fmc, freertos) and generate code. After, look in CubeIDE>Build Analyzer the memory usage for ram and flash. So generate code with touchgfx v4.13, through X-CUBE-TOUCHGFX, open touchgfx IDE and generate code there. Now touchgfx is enabled and you can see the new memory usage.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.