2021-04-18 9:41 PM
Hi,
I'm using a custom matrix orbital TFT display which is interfaced to the STM32H7B3-DK board through SPI. How to implement developed a UI from TouchGFX to the custom display. Referred to an FMC and SPI interface section, need better clarification. Please suggest a solution.
2021-04-19 1:44 AM
Hi,
Just to clarify the situation, you are working with an STM32H7B3-dk board and wish to change the display to your custom one ?
Have you started your project from scratch or did you use the application template for the STM32H7B3dk board available in TouchGFX Designer ? If the second scenario then you will need to modify the TouchGFX Generator in CubeMX and write a TouchGFX driver. Have a look and follow this guide on FMC and SPI Display Interface in the online documentation. Badreddine from ST also made a video on how to customize a TouchGFX template for STM32H7B3-dk boards. Even though he is not using the same display interface as you the main steps are the same. You can also have a look at the application template of the STM32G0nucleo board available in TouchGFX Designer. This board is also using a SPI display so you can look at the STM32CubeMXsettings and the code to have a better understanding of what to do.
/Romain
2021-04-20 2:06 AM
Do we need to write a driver's code for all the DK boards with built-in display and DK boards interfacing with the custom display while generating the project from cubeMX? I tried generating code for the STM32H7B3I-DK board (for built-in display) BSP driver files not generated when I generated code from the cubeMX and while debugging it is going to hardfault.
If you generate the code from touch GFX no issues everything working fine.
2021-04-20 6:15 AM
Hi,
When you create a project with an application template for an ST development board you will have a preconfigured project where we did all those steps for you. This is why you are missing the BSP files for example like you said.
/Romain
2021-04-20 10:22 PM
Hi Romain,
Can u please tell me how to get the BSP files and any other drivers files for the custom display when we create the project from the cubeMX.
/Megh
2021-04-20 11:35 PM
Well that depends :grinning_face_with_sweat: For custom hardware you either have to write them yourself or get them from someone who did it. For ST development kits you can get them under the folder <user name>/STM32Cube/Repository/<FW package you are looking for, like the FW_H7_V1.9.0>/Drivers.
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.