2021-11-21 7:17 AM
I'm working on a project using touchGfx and expected to be running on a WB55 processor (this is not important, except for that there is no WB55 based existing demo for touchGfx).
So i used STM32MX to configure some basic items, amongst which the fact i'm using Touchgfx.
Then i went into TouchGfx Designer to design the UI interface and flow.
The code compile and works perfectly as long as i was building for the simulator.
Now that i"m happy with the result in the simulator, next step is to compile and run for the hardware target based on WB55.
I know i'll soon or later have to write some low level code for instance for the LCD display and the TouchScreen, but i wanted to already get a first compile ( even not working or even with some errors) from STM32IDE. So i went into STM32MX and generate code (again, just in case).
Then i launch STM32IDE, import the project. I can see all the files (core, drivers, middleware, touchGfx) and inside TouchGfx i see all the files i wrote that are running fine with the simulator.
The problem is when i start compiling, almost no files from TouchGfx are being compiled. The drivers compile, the Core compiles, the touchGfx/App/app_toucgfx.c is being compiled. But none of the files inside TouchGfx/generated or TouchGfx/gui or TouchGfx/target are beling build/compiled and of course the build process fails because of undefined references.
So my question is how can i build my project (using touchgfx) from STM32IDE ?
Btw, i also tried to generate the code for IAR (>8.20) and there also all the TouchGfx related files are not compiled (they even don't appear in the project view.
Thanks for any pointers toward a solution.
Solved! Go to Solution.
2021-11-25 6:30 AM
Hello @LVers.1 ,
You don't have to share the whole project, I understand that it may contain some private work. What I need is a simple project (can be done by anyone) that shows the issue you are facing. You can create a new one and leave it empty. The GUI doesn't have to be complete.
Regards,
Sara.
2021-11-25 7:22 AM
Sara,
I think i could solve my issue, thanks to you.
As suggested i started a new minimal project to demonstrate the issue and, o suprise, there it works.
So i started to compare that project with my project having the issue and i saw that there were actually 2 .project and 2 .cproject file .
One set of file is located in project/STM32CubeIDE and i believe this is the right place and there was another set of files in project/ (project top level directory). I deleted those 2 files and suddenly it compiles fine from inside STM32IDE !
Thanks for the support. I must admit i was probably too lazy to make the new project by myself, so thanks for pushing me doing it :)
Stay tuned, i'll probably come back very soon with new questions,
Laurent
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.