2021-11-12 9:21 PM
I am working on touchgfx LCD. I need a a support to develop our custom application.
i have seen touchgfx API functions setup screen but i need example for better understanding.
2021-11-13 1:13 AM
application().gotoXXXXXScreenNoTransition();
2021-11-13 1:28 AM
Thank you but i have seen below information
switchScreen
virtual void switchScreen(Screen *newScreen)Switch to another Screen.Will call tearDownScreen on current Screen before switching, and subsequently call setupScreen and draw automatically for the new Screen.Parameters:newScreenA pointer to the new screen.
how can i use this to switch from one screen to other
virtual void switchScreen(Screen *newScreen)
2021-11-13 2:57 AM
I am not getting this gotoScreen5ScreenNoTransition() in application.gotoScreen5ScreenNoTransition(); with out interaction.
I do not want to add interaction so at that time what should i do for screen change ?
2021-11-13 4:03 AM
I dont check 4.18 , but every screen have in application Base generated NoTransition goto. Check it. Interaction dummy you need only for animated transition changes.
2021-11-13 4:18 AM
I am using 4.17.0 Base generated NoTransition goto not generated when add screen only
but generated whenvever adding screen change interaction
2021-11-13 4:24 AM
You check file FrontendApplicationBase.cpp?
2021-11-13 4:50 AM
yes
i checked that file
not generated Base generated NoTransition in FrontendApplicationBase.cpp if i just add screen simply.
so How can i change screen with out this application().gotoXXXXXScreenNoTransition();. finally i got a error.
2021-11-13 4:52 AM
i am checking Screen Transition Declarations in FrontendApplicationBase.cpp ..Is it right?
2021-11-13 4:57 AM
I have only one no empty screen in app no interactions and file in v 4.17
/*********************************************************************************/
/********** THIS FILE IS GENERATED BY TOUCHGFX DESIGNER, DO NOT MODIFY ***********/
/*********************************************************************************/
#include <new>
#include <gui_generated/common/FrontendApplicationBase.hpp>
#include <gui/common/FrontendHeap.hpp>
#include <touchgfx/transitions/NoTransition.hpp>
#include <texts/TextKeysAndLanguages.hpp>
#include <touchgfx/Texts.hpp>
#include <touchgfx/hal/HAL.hpp>
#include <platform/driver/lcd/LCD16bpp.hpp>
#include <gui/screen1_screen/Screen1View.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
using namespace touchgfx;
FrontendApplicationBase::FrontendApplicationBase(Model& m, FrontendHeap& heap)
: touchgfx::MVPApplication(),
transitionCallback(),
frontendHeap(heap),
model(m)
{
touchgfx::HAL::getInstance()->setDisplayOrientation(touchgfx::ORIENTATION_LANDSCAPE);
reinterpret_cast<touchgfx::LCD16bpp&>(touchgfx::HAL::lcd()).enableTextureMapperAll();
}
/*
* Screen Transition Declarations
*/
// Screen1
void FrontendApplicationBase::gotoScreen1ScreenNoTransition()
{
transitionCallback = touchgfx::Callback<FrontendApplicationBase>(this, &FrontendApplication::gotoScreen1ScreenNoTransitionImpl);
pendingScreenTransitionCallback = &transitionCallback;
}
void FrontendApplicationBase::gotoScreen1ScreenNoTransitionImpl()
{
touchgfx::makeTransition<Screen1View, Screen1Presenter, touchgfx::NoTransition, Model >(¤tScreen, ¤tPresenter, frontendHeap, ¤tTransition, &model);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.