2019-01-13 8:57 PM
I downloaded the latest STM32 Cube package for the F4 (ver 1.23.0). I'm trying to build Projects\STM32469I-Discovery\Demonstrations\TouchGFX\SW4STM32\STM32469I-Discovery using the free System Workbench (latest 32-bit version 2.7 on Windows 10). The build goes ok and I can run it but I don't see anything on my STM32F469I-DISCO display. Should this work?
Is there a way to build and re-load the code that came originally with the STM32F469I-DISCO eval board?
2019-01-16 8:22 AM
Hello @jay2399 ,
As recommended in the readme.txt file of the demonstration example, please use the STM32CubeProgrammer utility to flash the application's HEX file to the STM32 target.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.