2022-04-19 4:13 AM
I am makeing a gauge background out of many circle widgets. I dont want to use static immage background because the position of segments can change depending on the maximum rpm.
I have create this in TouchGFX designer and for each circle widget Designer created also a painter. Therefor there are many painter that have the same color configuration. Is it possible to eliminate some widgets and/or painters to reduce the memory consumption.
part of generated code CustomGaugeBackgroundBase.cpp
segmentBig1.setPosition(0, 0, 494, 426);
segmentBig1.setCenter(247, 246);
segmentBig1.setRadius(235);
segmentBig1.setLineWidth(22);
segmentBig1.setArc(-136, -133);
segmentBig1.setCapPrecision(180);
segmentBig1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig1.setPainter(segmentBig1Painter);
segmentBig8.setPosition(0, 0, 494, 426);
segmentBig8.setCenter(247, 246);
segmentBig8.setRadius(235);
segmentBig8.setLineWidth(22);
segmentBig8.setArc(134, 137);
segmentBig8.setCapPrecision(180);
segmentBig8Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig8.setPainter(segmentBig8Painter);
segmentBig2.setPosition(0, 0, 494, 426);
segmentBig2.setCenter(247, 246);
segmentBig2.setRadius(235);
segmentBig2.setLineWidth(22);
segmentBig2.setArc(-98, -95);
segmentBig2.setCapPrecision(180);
segmentBig2Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig2.setPainter(segmentBig2Painter);
segmentBig3.setPosition(0, 0, 494, 426);
segmentBig3.setCenter(247, 246);
segmentBig3.setRadius(235);
segmentBig3.setLineWidth(22);
segmentBig3.setArc(-59, -56);
segmentBig3.setCapPrecision(180);
segmentBig3Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig3.setPainter(segmentBig3Painter);
segmentBig4.setPosition(0, 0, 494, 426);
segmentBig4.setCenter(247, 246);
segmentBig4.setRadius(235);
segmentBig4.setLineWidth(22);
segmentBig4.setArc(-21, -18);
segmentBig4.setCapPrecision(180);
segmentBig4Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig4.setPainter(segmentBig4Painter);
segmentBig5.setPosition(0, 0, 494, 426);
segmentBig5.setCenter(247, 246);
segmentBig5.setRadius(235);
segmentBig5.setLineWidth(22);
segmentBig5.setArc(18, 21);
segmentBig5.setCapPrecision(180);
segmentBig5Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig5.setPainter(segmentBig5Painter);
segmentBig6.setPosition(0, 0, 494, 426);
segmentBig6.setCenter(247, 246);
segmentBig6.setRadius(235);
segmentBig6.setLineWidth(22);
segmentBig6.setArc(57, 60);
segmentBig6.setCapPrecision(180);
segmentBig6Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig6.setPainter(segmentBig6Painter);
segmentBig7.setPosition(0, 0, 494, 426);
segmentBig7.setCenter(247, 246);
segmentBig7.setRadius(235);
segmentBig7.setLineWidth(22);
segmentBig7.setArc(95, 98);
segmentBig7.setCapPrecision(180);
segmentBig7Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentBig7.setPainter(segmentBig7Painter);
circleOut.setPosition(0, 0, 494, 426);
circleOut.setCenter(247, 246);
circleOut.setRadius(245);
circleOut.setLineWidth(3);
circleOut.setArc(-136, 135);
circleOut.setCapPrecision(180);
circleOutPainter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
circleOut.setPainter(circleOutPainter);
segmentSmall1_1.setPosition(0, 0, 494, 426);
segmentSmall1_1.setCenter(247, 246);
segmentSmall1_1.setRadius(240);
segmentSmall1_1.setLineWidth(10);
segmentSmall1_1.setArc(-128, -126);
segmentSmall1_1.setCapPrecision(180);
segmentSmall1_1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall1_1.setPainter(segmentSmall1_1Painter);
segmentSmall1_2.setPosition(0, 0, 494, 426);
segmentSmall1_2.setCenter(247, 246);
segmentSmall1_2.setRadius(240);
segmentSmall1_2.setLineWidth(10);
segmentSmall1_2.setArc(-121, -119);
segmentSmall1_2.setCapPrecision(180);
segmentSmall1_2Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall1_2.setPainter(segmentSmall1_2Painter);
segmentSmall1_3.setPosition(0, 0, 494, 426);
segmentSmall1_3.setCenter(247, 246);
segmentSmall1_3.setRadius(240);
segmentSmall1_3.setLineWidth(10);
segmentSmall1_3.setArc(-111, -113);
segmentSmall1_3.setCapPrecision(180);
segmentSmall1_3Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall1_3.setPainter(segmentSmall1_3Painter);
segmentSmall1_4.setPosition(0, 0, 494, 426);
segmentSmall1_4.setCenter(247, 246);
segmentSmall1_4.setRadius(240);
segmentSmall1_4.setLineWidth(10);
segmentSmall1_4.setArc(-103, -105);
segmentSmall1_4.setCapPrecision(180);
segmentSmall1_4Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall1_4.setPainter(segmentSmall1_4Painter);
segmentSmall2_1.setPosition(0, 0, 494, 426);
segmentSmall2_1.setCenter(247, 246);
segmentSmall2_1.setRadius(240);
segmentSmall2_1.setLineWidth(10);
segmentSmall2_1.setArc(-90, -88);
segmentSmall2_1.setCapPrecision(180);
segmentSmall2_1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall2_1.setPainter(segmentSmall2_1Painter);
segmentSmall2_2.setPosition(0, 0, 494, 426);
segmentSmall2_2.setCenter(247, 246);
segmentSmall2_2.setRadius(240);
segmentSmall2_2.setLineWidth(10);
segmentSmall2_2.setArc(-80, -82);
segmentSmall2_2.setCapPrecision(180);
segmentSmall2_2Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall2_2.setPainter(segmentSmall2_2Painter);
segmentSmall2_3.setPosition(0, 0, 494, 426);
segmentSmall2_3.setCenter(247, 246);
segmentSmall2_3.setRadius(240);
segmentSmall2_3.setLineWidth(10);
segmentSmall2_3.setArc(-73, -75);
segmentSmall2_3.setCapPrecision(180);
segmentSmall2_3Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall2_3.setPainter(segmentSmall2_3Painter);
segmentSmall2_4.setPosition(0, 0, 494, 426);
segmentSmall2_4.setCenter(247, 246);
segmentSmall2_4.setRadius(240);
segmentSmall2_4.setLineWidth(10);
segmentSmall2_4.setArc(-65, -67);
segmentSmall2_4.setCapPrecision(180);
segmentSmall2_4Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall2_4.setPainter(segmentSmall2_4Painter);
segmentSmall3_1.setPosition(0, 0, 494, 426);
segmentSmall3_1.setCenter(247, 246);
segmentSmall3_1.setRadius(240);
segmentSmall3_1.setLineWidth(10);
segmentSmall3_1.setArc(-49, -51);
segmentSmall3_1.setCapPrecision(180);
segmentSmall3_1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
segmentSmall3_1.setPainter(segmentSmall3_1Painter);
Solved! Go to Solution.
2022-04-19 6:42 AM
Hello manto.1,
Unfortunately there's not too many option. The only thing that you can maybe try is to do a half of your image and try to do a "mirroring" on it. It should be possible with an AbstractPainter but I never tried it. But I'm not sure if you'll always have a symmetry on your gauge, if not, this solution will not work.
Else I don't see other solution than changing your scale instead of changing the position of your segments, or use a static image background.
/Osman
2022-04-19 6:42 AM
Hello manto.1,
Unfortunately there's not too many option. The only thing that you can maybe try is to do a half of your image and try to do a "mirroring" on it. It should be possible with an AbstractPainter but I never tried it. But I'm not sure if you'll always have a symmetry on your gauge, if not, this solution will not work.
Else I don't see other solution than changing your scale instead of changing the position of your segments, or use a static image background.
/Osman
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.