2022-04-14 8:03 AM
I try add to pnucleo WB55 project touchgfx package and result is
../Drivers/CMSIS/Device/ST/STM32WBxx/Include/stm32wb55xx.h:1084:29: error: expected identifier before '(' token
1084 | #define LCD ((LCD_TypeDef *) LCD_BASE)
| ^
../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp:44:66: note: in expansion of macro 'LCD'
44 | TouchGFXGeneratedHAL(touchgfx::DMA_Interface& dma, touchgfx::LCD& display, touchgfx::TouchController& tc, uint16_t width, uint16_t height) :
| ^~~
../Drivers/CMSIS/Device/ST/STM32WBxx/Include/stm32wb55xx.h:961:31: error: expected ')' before '(' token
961 | #define LCD_BASE (APB1PERIPH_BASE + 0x00002400UL)
| ^
../Drivers/CMSIS/Device/ST/STM32WBxx/Include/stm32wb55xx.h:1084:46: note: in expansion of macro 'LCD_BASE'
1084 | #define LCD ((LCD_TypeDef *) LCD_BASE)
| ^~~~~~~~
../TouchGFX/target/generated/TouchGFXGeneratedHAL.hpp:44:66: note: in expansion of macro 'LCD'
44 | TouchGFXGeneratedHAL(touchgfx::DMA_Interface& dma, touchgfx::LCD& display, touchgfx::TouchController& tc, uint16_t width, uint16_t height) :
|and next more errors around defined LCD.
Primary colision is in generated files = hard to edit.
Howto solve this ?
TouchGFXGeneratedHAL(touchgfx::DMA_Interface& dma, touchgfx::LCD& display, touchgfx::TouchController& tc, uint16_t width, uint16_t height) :
touchgfx::HAL(dma, display, tc, width, height)
{
}
Solved! Go to Solution.
2022-04-19 7:00 AM
WB 1.12.1, TGFX 4.17.0 , IDE 1.7.0
My solution
#ifndef TouchGFXGeneratedHAL_HPP
#define TouchGFXGeneratedHAL_HPP
#include <touchgfx/hal/HAL.hpp>
#undef LCD
2022-04-19 3:20 AM
Hello MM..1,
Can you give more information about your configuration please ?
This bug was identified before TouchGFX Designer 4.19.0, and have been resolved since.
/Osman
2022-04-19 7:00 AM
WB 1.12.1, TGFX 4.17.0 , IDE 1.7.0
My solution
#ifndef TouchGFXGeneratedHAL_HPP
#define TouchGFXGeneratedHAL_HPP
#include <touchgfx/hal/HAL.hpp>
#undef LCD
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.