2019-03-21 4:01 AM
The ability to package code into application templates is a great feature for preparing platform-specific projects, but it mainly seems to involve adding pre-existing files that are incorporated into the project skeleton. But is there any way to add additional code to the classes that are generated when a new TouchGFX project is created?
Say, for instance, that I wanted the screen-class to inherit from another base class (as a way of seamlessly extending the screen-class functionality) automatically at project creation. Is it possible to do this in the application template rather than having to do it for every new project?
2019-04-02 12:54 AM
There's no direct support for this. In your post-generate command (.touchgfx file) you could call a script to modify each generated file to inherit from another class.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.