2019-08-05 12:13 AM
Hello,
I use stm32f429 disco board which has IS42S16400J 64Mb SDRAM,
so I use SDRAM for frame buffer.
Is there any opportunity to know how much SDRAM memory my application needs?
and how much I use at the moment?
Thank you,
Anton
Solved! Go to Solution.
2019-08-05 12:46 AM
Hi @qqAnton,
Ah, i responded to what the screen allocation uses.
The frame buffer allocation uses:
height * width * bitdepth * number of framebuffers
The bitdepth is in bytes used:
24 bitdepth: 3
16 bitdepth: 2
In this configuration the application is configured to use double buffering and an additional animation storage, so three framebuffers
height * width * bitdepth * 3
These frame buffers are located sequential starting from 0xD0000000.
the prototype for setFramebufferStartAddress
void setFrameBufferStartAddress(void* adr, uint16_t depth = 16, bool useDoubleBuffering = true, bool useAnimationStorage = true)
/Anders
2019-08-05 12:21 AM
Hi @qqAnton,
For the TouchGFX application you can look in the map file generated and look for: FrontendHeap::getInstance()::instance
Below is from a gcc map file, here the ram usage of the touchgfx gui application is 0x4bd4 located at 0x24000c20.
.bss._ZZN12FrontendHeap11getInstanceEvE8instance
0x24000c20 0x4bd4 TouchGFX/build/STM32H747I_DISCO/TouchGFX/target/BoardConfiguration.o
0x24000c20 FrontendHeap::getInstance()::instance
This is statically allocated, TouchGFX will not allocate on runtime.
how much I use at the moment?
If you are using a OS, I suggest you enable the OS' watermark settings to check the current usage.
/Anders
2019-08-05 12:29 AM
@Anders Nedergaard PETERSEN thank you for the answer,
I am sorry, maybe I understand something wrong,
but I want to know how much SDRAM I use which starts from 0xD0000000,
static uint32_t frameBuf0 = (uint32_t)(0xd0000000);
hal.setFrameBufferStartAddress((uint16_t*)frameBuf0, bitdepth ,true , true);
2019-08-05 12:46 AM
Hi @qqAnton,
Ah, i responded to what the screen allocation uses.
The frame buffer allocation uses:
height * width * bitdepth * number of framebuffers
The bitdepth is in bytes used:
24 bitdepth: 3
16 bitdepth: 2
In this configuration the application is configured to use double buffering and an additional animation storage, so three framebuffers
height * width * bitdepth * 3
These frame buffers are located sequential starting from 0xD0000000.
the prototype for setFramebufferStartAddress
void setFrameBufferStartAddress(void* adr, uint16_t depth = 16, bool useDoubleBuffering = true, bool useAnimationStorage = true)
/Anders
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.