2020-07-30 10:19 PM
I wonder whether it is feasible to use 3D GPU on stm32MP1 instead of DMA2D?
Solved! Go to Solution.
2020-08-28 3:06 AM
It would be possible, yes. It's not something we have attempted yet, because the MP1 is a bit out of scope for us. Granted, you could run TouchGFX on the M4. I've only done some preliminary tests, but since it's not a priority for us i haven't dedicated any time to it.
To be able to use it with the current implementation of TouchGFX, you'd have to use the current DMA interface which uses BlitOp's. Check out the BlitOp Type. It specifies a src, a dst, steps and loops, etc.
struct BlitOp
{
uint32_t operation; ///< The operation to perform @see BlitOperations
const uint16_t* pSrc; ///< Pointer to the source (pixels or indexes)
const uint16_t* pClut; ///< Pointer to the source CLUT entires
uint16_t* pDst; ///< Pointer to the destination
uint16_t nSteps; ///< The number of pixels in a line
uint16_t nLoops; ///< The number of lines
uint16_t srcLoopStride; ///< The number of bytes to stride the source after every loop
uint16_t dstLoopStride; ///< The number of bytes to stride the destination after every loop
colortype color; ///< Color to fill
uint16_t alpha; ///< The alpha to use
uint16_t srcFormat; ///< The source format @see Bitmap::BitmapFormat
uint16_t dstFormat; ///< The destination format @see Bitmap::BitmapFormat
};For any specific features, like rotation and scaling you could create your own custom widgets and then implement the functionality in the ::draw() function hooking directly into the GPU API. But you need to come up with a mechanism that protects the framebuffer in the same way that we do for DMA2D. And this is a bit different on Linux. Not to mention that you need a new, customized HAL to run on top of Linux. I have one that runs on a Raspberry pi, but it's highly unofficial.
/Martin
2020-07-31 5:06 AM
Hello,
TouchGFX is not made for real 3D rendering. The framebuffer is only 2D.
Also, we do not have any TouchGFX example running on stm32MP1.
What you are trying to do has never been thought of, so unfortunately, we cannot help you on that.
/Alexandre
2020-08-28 3:06 AM
It would be possible, yes. It's not something we have attempted yet, because the MP1 is a bit out of scope for us. Granted, you could run TouchGFX on the M4. I've only done some preliminary tests, but since it's not a priority for us i haven't dedicated any time to it.
To be able to use it with the current implementation of TouchGFX, you'd have to use the current DMA interface which uses BlitOp's. Check out the BlitOp Type. It specifies a src, a dst, steps and loops, etc.
struct BlitOp
{
uint32_t operation; ///< The operation to perform @see BlitOperations
const uint16_t* pSrc; ///< Pointer to the source (pixels or indexes)
const uint16_t* pClut; ///< Pointer to the source CLUT entires
uint16_t* pDst; ///< Pointer to the destination
uint16_t nSteps; ///< The number of pixels in a line
uint16_t nLoops; ///< The number of lines
uint16_t srcLoopStride; ///< The number of bytes to stride the source after every loop
uint16_t dstLoopStride; ///< The number of bytes to stride the destination after every loop
colortype color; ///< Color to fill
uint16_t alpha; ///< The alpha to use
uint16_t srcFormat; ///< The source format @see Bitmap::BitmapFormat
uint16_t dstFormat; ///< The destination format @see Bitmap::BitmapFormat
};For any specific features, like rotation and scaling you could create your own custom widgets and then implement the functionality in the ::draw() function hooking directly into the GPU API. But you need to come up with a mechanism that protects the framebuffer in the same way that we do for DMA2D. And this is a bit different on Linux. Not to mention that you need a new, customized HAL to run on top of Linux. I have one that runs on a Raspberry pi, but it's highly unofficial.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.