2019-06-01 4:21 AM
I currently have a TFT LGDP display and I can't figure out how to hook it up with my stmf303 re.
2019-06-02 9:56 AM
An 8080/6800 type bus should be within grasp, most of the requirements tend to be setup/hold times with respect to edges of latching signals.
2019-06-02 2:41 PM
I guess you're right. The essential timings don't have maximums. It just would be a lot slower than with F(S)MC, but way faster than with SPI. Too bad bit banging doesn't work with DMA - like ChromArt...
2019-06-02 3:59 PM
Done some interesting things here with pattern buffers, GPIO, TIM and DMA.
Anyway the question has been very poorly framed/scoped. Assuming some NUCLEO-F303RE, and some random display board. When playing "Will It Blend" we might do better with a lot more precision.
Historically people have interfaced 16x2 LCD displays via GPIO and bit banged. I've got some nice OLEDs I'm driving through I2C (SSD 1306/1309).
SPI is also an option, but ST's implementation is frankly less than ideal.
2019-06-04 3:08 PM
The problem is that I'm trying to launch a tft lcd for the first time and I'm not sure datasheet will provide me enough hints as it is designed in a roundabout way(at least it seems like that to me). Did anybody make a similar project?
2019-06-04 9:18 PM
I wrote some code for a QVGA-display using 8080-interface (RGB565). I used FMC NAND of F427, because otherwise I couldn't get the data hold time long enough.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.