2021-03-10 8:41 PM
A singular slider works fine in the page. I've tried many callback/handler methods (individual for each slider, combined with cases), but can't seem to be able to fix the issue.
See my attached pageSetupView.cpp and pageSetupView.hpp functions pertaining to the sliders.
void ZoneSetupView::setupScreen()
{
//Zone 1 Slider Definition
zone1Temp.setXY(120, 60);
zone1Temp.setBitmaps(touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_ID), touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_FILLED_ID), touchgfx::Bitmap(BITMAP_SLIDER_KNOB_CIRCLE_ID));
zone1Temp.setupHorizontalSlider(14, 14, 0, 0, 200);
zone1Temp.setValueRange(50, 250);
zone1Temp.setValue(100);
zone1Temp.setVisible(false);
add(zone1Temp);
zone1Temp.setStartValueCallback(zonetempsliderValueStartedChangeCallback);
zone1Temp.setNewValueCallback(zonetempsliderValueChangedCallback);
zone1Temp.setStopValueCallback(zonetempsliderValueConfirmedCallback);
textZone1Temp.setPosition(360, 65, 115, 46);
textZone1Temp.setColor(Color::getColorFrom24BitRGB(255, 255, 255));
textZone1Temp.setLinespacing(0);
textZone1TempBuffer[0] = 0;
textZone1Temp.setWildcard(textZone1TempBuffer);
textZone1Temp.setTypedText(TypedText(T_ZONETEMP));
textZone1Temp.setVisible(false);
add(textZone1Temp);
//Zone 2 Slider Definition
zone2Temp.setXY(120, 100);
zone2Temp.setBitmaps(touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_ID), touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_FILLED_ID), touchgfx::Bitmap(BITMAP_SLIDER_KNOB_CIRCLE_ID));
zone2Temp.setupHorizontalSlider(14, 14, 0, 0, 200);
zone2Temp.setValueRange(50, 250);
zone2Temp.setValue(100);
zone2Temp.setVisible(false);
add(zone2Temp);
zone2Temp.setStartValueCallback(zonetempsliderValueStartedChangeCallback);
zone2Temp.setNewValueCallback(zonetempsliderValueChangedCallback);
zone2Temp.setStopValueCallback(zonetempsliderValueConfirmedCallback);
textZone2Temp.setPosition(360, 105, 115, 46);
textZone2Temp.setColor(Color::getColorFrom24BitRGB(255, 255, 255));
textZone2Temp.setLinespacing(0);
textZone2TempBuffer[0] = 0;
textZone2Temp.setWildcard(textZone2TempBuffer);
textZone2Temp.setTypedText(TypedText(T_ZONETEMP));
textZone2Temp.setVisible(false);
add(textZone2Temp);
//Zone 3 Slider Definition
zone3Temp.setXY(120, 140);
zone3Temp.setBitmaps(touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_ID), touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_FILLED_ID), touchgfx::Bitmap(BITMAP_SLIDER_KNOB_CIRCLE_ID));
zone3Temp.setupHorizontalSlider(14, 14, 0, 0, 200);
zone3Temp.setValueRange(50, 250);
zone3Temp.setValue(100);
zone3Temp.setVisible(false);
add(zone3Temp);
zone3Temp.setStartValueCallback(zonetempsliderValueStartedChangeCallback);
zone3Temp.setNewValueCallback(zonetempsliderValueChangedCallback);
zone3Temp.setStopValueCallback(zonetempsliderValueConfirmedCallback);
textZone3Temp.setPosition(360, 145, 115, 46);
textZone3Temp.setColor(Color::getColorFrom24BitRGB(255, 255, 255));
textZone3Temp.setLinespacing(0);
textZone3TempBuffer[0] = 0;
textZone3Temp.setWildcard(textZone3TempBuffer);
textZone3Temp.setTypedText(TypedText(T_ZONETEMP));
textZone3Temp.setVisible(false);
add(textZone3Temp);
//Zone 4 Slider Definition
zone4Temp.setXY(120, 180);
zone4Temp.setBitmaps(touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_ID), touchgfx::Bitmap(BITMAP_SLIDER_BACKGROUND_FILLED_ID), touchgfx::Bitmap(BITMAP_SLIDER_KNOB_CIRCLE_ID));
zone4Temp.setupHorizontalSlider(14, 14, 0, 0, 200);
zone4Temp.setValueRange(50, 250);
zone4Temp.setValue(100);
zone4Temp.setVisible(false);
add(zone4Temp);
zone4Temp.setStartValueCallback(zonetempsliderValueStartedChangeCallback);
zone4Temp.setNewValueCallback(zonetempsliderValueChangedCallback);
zone4Temp.setStopValueCallback(zonetempsliderValueConfirmedCallback);
textZone4Temp.setPosition(360, 185, 115, 46);
textZone4Temp.setColor(Color::getColorFrom24BitRGB(255, 255, 255));
textZone4Temp.setLinespacing(0);
textZone4TempBuffer[0] = 0;
textZone4Temp.setWildcard(textZone4TempBuffer);
textZone4Temp.setTypedText(TypedText(T_ZONETEMP));
textZone4Temp.setVisible(false);
add(textZone4Temp);
slideMenuElementSelectedHandler(slideMenu);
zonetempsliderValueConfirmedCallbackHandler(zone1Temp, zone1Temp.getValue());
zonetempsliderValueConfirmedCallbackHandler(zone2Temp, zone2Temp.getValue());
zonetempsliderValueConfirmedCallbackHandler(zone3Temp, zone3Temp.getValue());
zonetempsliderValueConfirmedCallbackHandler(zone4Temp, zone4Temp.getValue());
ZoneSetupViewBase::setupScreen();
}
void ZoneSetupView::slideMenuElementSelectedHandler(const VerticalSlideMenu& menu)
{
int selectedElement = slideMenu.getSelectedElementIndex();
// Setup menu up/down button. First set default then handle special cases
menuUp.setBitmaps(Bitmap(BITMAP_CONTROL_MENU_ARROW_UP_ID), Bitmap(BITMAP_CONTROL_MENU_ARROW_UP_PRESSED_ID));
menuDown.setBitmaps(Bitmap(BITMAP_CONTROL_MENU_ARROW_DOWN_ID), Bitmap(BITMAP_CONTROL_MENU_ARROW_DOWN_PRESSED_ID));
menuUp.setTouchable(true);
menuDown.setTouchable(true);
if (selectedElement == 0)
{
menuUp.setBitmaps(Bitmap(BITMAP_CONTROL_MENU_ARROW_UP_INACTIVE_ID), Bitmap(BITMAP_CONTROL_MENU_ARROW_UP_INACTIVE_ID));
menuUp.setTouchable(false);
}
else if (selectedElement == slideMenu.getSize() - 1)
{
menuDown.setBitmaps(Bitmap(BITMAP_CONTROL_MENU_ARROW_DOWN_INACTIVE_ID), Bitmap(BITMAP_CONTROL_MENU_ARROW_DOWN_INACTIVE_ID));
menuDown.setTouchable(false);
}
// Expand the active area of the buttons to make them easier to activate
menuUp.setWidth(menuUp.getWidth() + 30);
menuDown.setWidth(menuDown.getWidth() + 30);
menuUp.invalidate();
menuDown.invalidate();
// Set the chosen control visible
zone1Temp.setVisible(selectedElement == 0);
zone2Temp.setVisible(selectedElement == 0);
zone3Temp.setVisible(selectedElement == 0);
zone4Temp.setVisible(selectedElement == 0);
textZone1Temp.setVisible(selectedElement == 0);
textZone2Temp.setVisible(selectedElement == 0);
textZone3Temp.setVisible(selectedElement == 0);
textZone4Temp.setVisible(selectedElement == 0);
textZone1Temp.invalidate();
textZone2Temp.invalidate();
textZone3Temp.invalidate();
textZone4Temp.invalidate();
zone1Temp.invalidate();
zone2Temp.invalidate();
zone3Temp.invalidate();
zone4Temp.invalidate();
}
void ZoneSetupView::zonetempsliderValueConfirmedCallbackHandler(const Slider& src, int value)
{
if (&src == &zone1Temp)
{
//execute code whenever the slider stops the changing value.
//update slider and temperature text
zone1Temp.setValue(value);
Unicode::snprintf(textZone1TempBuffer, 4, "%d", value);
//textZone1Temp.invalidate();
}
else if(&src == &zone2Temp)
{
//execute code whenever the slider stops the changing value.
//update slider and temperature text
zone2Temp.setValue(value);
Unicode::snprintf(textZone2TempBuffer, 4, "%d", value);
//textZone2Temp.invalidate();
}
else if(&src == &zone3Temp)
{
//execute code whenever the slider stops the changing value.
//update slider and temperature text
zone3Temp.setValue(value);
Unicode::snprintf(textZone3TempBuffer, 4, "%d", value);
//textZone3Temp.invalidate();
}
else if(&src == &zone4Temp)
{
//execute code whenever the slider stops the changing value.
//update slider and temperature text
zone4Temp.setValue(value);
Unicode::snprintf(textZone4TempBuffer, 4, "%d", value);
//textZone4Temp.invalidate();
}
textZone1Temp.invalidate();
textZone2Temp.invalidate();
textZone3Temp.invalidate();
textZone4Temp.invalidate();
}
Maybe I'm missing something? Thanks!
2021-03-11 4:38 AM
Hi,
The code is quite long so I didn't go though it entirely :grinning_face_with_sweat:, but this is definitely possible. The UI Template "Slider Example" available in TouchGFX Designer uses two sliders.
/Romain
2021-03-11 5:35 AM
Hi Romain,
I used the "Slider Example" as the building blocks for this. However when adding additional similar like (all horizontal sliders) my example fails. Could it have anything to do with the same generic 'Slider' callbacks (setStartValueCallback, setNewValueCallback, setStopValueCallback) each referenced 4 times (for four sliders) like the following? If that's the case is there another way to notify when a slider has changed? I tried independently named callbacks for each zone too (i.e. zone1sliderValueStartedChangeCallback, zone1silderValueChangedCallback, zone1sliderValueConfirmedCallback).
zone1Temp.setStartValueCallback(zonetempsliderValueStartedChangeCallback);
zone1Temp.setNewValueCallback(zonetempsliderValueChangedCallback);
zone1Temp.setStopValueCallback(zonetempsliderValueConfirmedCallback);
zone2Temp.setStartValueCallback(zonetempsliderValueStartedChangeCallback);
zone2Temp.setNewValueCallback(zonetempsliderValueChangedCallback);
zone2Temp.setStopValueCallback(zonetempsliderValueConfirmedCallback);
//...etc.Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.