2025-02-20 12:38 AM
Hi Gfx Team,
Could you please implement drag&drop as an alternative to open a project.touchgfx ?
Thank you
Solved! Go to Solution.
2025-02-20 1:30 AM
The new incoming version of TouchGFX Designer will open way faster, so if it is just to avoid closing then re-opening TouchGFX Designer because it is slow, it won't be that important soon.
Perhaps the new incoming version would be a sufficient solution and opening a new project from "File" => "Open" would be a sufficient work around while waiting for the new version?
Regards,
2025-02-20 12:55 AM
Hello @ferro ,
In which case would the drag and drop be useful for you?
Do you want to be able to drag a .touchgfx project in the Designer main window at any time?
Do you want to be able to drag a .touchgfx file after clicking on "File" => "Open"?
Regards,
2025-02-20 1:07 AM
"be able to drag a .touchgfx project in the Designer main window at any time?"
This would be ideal.
2025-02-20 1:24 AM
Until now, I've always closed the Designer, clicked on the project.touchgfx and let the OS handle it. Very slow. MSVC IDE spoiled me with my expectations - its very fast.
I just noticed that keeping the Designer open and opening a project.touchgfx via [file > open] is lightning fast.
2025-02-20 1:30 AM
The new incoming version of TouchGFX Designer will open way faster, so if it is just to avoid closing then re-opening TouchGFX Designer because it is slow, it won't be that important soon.
Perhaps the new incoming version would be a sufficient solution and opening a new project from "File" => "Open" would be a sufficient work around while waiting for the new version?
Regards,
2025-02-20 1:35 AM
"opening a new project from "File" => "Open" would be a sufficient work around while waiting for the new version"
Yes, it is good as it is. Thanks.
2025-02-20 1:56 AM
My pleasure! :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.