2025-10-17 4:06 AM - edited 2025-10-17 5:50 AM
Hi,
I’d like to terminate the build process, but pressing F7 causes GfxDesigner(4.24.1) to crash.
2025-10-17 13:46:51,280 [1] WARN TouchGFXDomainModel.Texts.FontGetter: font already added. (path: HPSimplified_LtIt.ttf, name: HPSimplified_LtIt
2025-10-17 13:46:51,280 [1] WARN TouchGFXDomainModel.Texts.FontGetter: font already added. (path: HPSimplified_Rg.ttf, name: HPSimplified_Rg
2025-10-17 13:48:35,702 [26] ERROR TouchGFXDesigner.App: Invalid class
System.Management.ManagementException: Invalid class
at System.Management.ManagementException.ThrowWithExtendedInfo(ManagementStatus errorCode)
at System.Management.ManagementObjectCollection.ManagementObjectEnumerator.MoveNext()
at TouchGFXApplication.Executors.Executor.Cancel()
at TouchGFXApplication.MonitorCommands.RunSimulatorCommand.Cancel()
at TouchGFXApplication.TouchGFXApplication.<CancelCompile>b__38_0()
at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)
--- End of stack trace from previous location ---
at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)Is there any other way to do that ? A key combination ?
Thanks
2025-10-20 1:23 AM
Hello @ferro.
I am not aware of any other way to terminate the build except by pressing Cancel or F7 without closing TouchGFX Designer. However, I have never experienced issues with this.
Does the issue only occur when you cancel the simulator build, or does it also happen with Generate Code and Run Target (if available)? Could you try to replicate the issue in TouchGFX 4.26.0?
Best regards,
Johan
2025-10-20 12:19 PM
Thanks @JohanAstrup
With 4.24.1, I press F5 and the Designer starts to generate code. Pressing F7 during that causes the Designer to crashe. So it does when I press F7 while compiling. I run simulation only.
"Could you try to replicate the issue in TouchGFX 4.26.0?"
I will.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.