2025-06-11 8:07 AM
Dear Gfx Team,
I worked on a project using CubeIDE 1.17.0 and GfxDesigner 4.24.1.
I installed and un-installed 4.25.0.
Now, when I open \TouchGFX\mcu_project.touchgfx with 4.24.1 and press F4/F5, the version in \mcu_project.ioc is changed from 4.24.1 to 4.25.0.
Why is that and how to stop it please ?
Thank you
Solved! Go to Solution.
2025-06-16 4:46 AM
Ok, tell me how it goes.
Regards,
2025-06-16 4:58 AM
I can run project in 4.25.0.
The error in 4.24.1 is still there but message has changed, no mention of 4.25.0
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
C:/TouchGFX/4.24.1/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems.rb:281:in `find_spec_for_exe': can't find gem touchgfx-cli (>= 0.a) with executable touchgfx (Gem::GemNotFoundException)
from C:/TouchGFX/4.24.1/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems.rb:300:in `activate_bin_path'
from C:/TouchGFX/4.24.1/env/MinGW/msys/1.0/Ruby30-x64/bin/touchgfx:23:in `<main>'
Failed
Failed
I'll run 4.24.1 installer and try 'Repair' intallation.
2025-06-16 5:29 AM
>> I'll run 4.24.1 installer and try 'Repair' intallation.
Running 'Repair' seems to fix the error in my original question and also error in creating new project in 4.24.1.
I'll mark this post as the answer in few days if there is no problem.
Thanks for help @GaetanGodart
2025-06-16 5:34 AM
Ok, great to hear! :)
I did not help that much haha, you did all the work. ^^
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.