2019-07-10 5:36 AM
Hello
I want to know the MCU Load, so I found this function
McuLoad = touchgfx::HAL::getInstance()->getMCULoadPct();I call it in
void Model::tick()But I always get 0, whatever I do it alwsys returns zero, so I don't think it's working well,
so, how could I resolve the problem? maybe I should call it from another place?
Thank you
Anton
2019-07-10 6:07 AM
Hi @qqAnton,
First of all you must enable MCU load calculation in your HAL configuration. Which platform are you using?
//From BoardConfiguration.cpp
STM32F7Instrumentation mcuInstr;
...
void touchgfx_init()
{
...
mcuInstr.init();
hal.setMCUInstrumentation(&mcuInstr);
hal.enableMCULoadCalculation(true);
...
2019-07-10 10:09 PM
I use stm32f429i-disco.
I have these functions in my BoardConfiguration.cpp
mcuInstr.init();
//Set MCU instrumentation and Load calculation
hal.setMCUInstrumentation(&mcuInstr);
hal.enableMCULoadCalculation(true);But it is not working
2019-07-11 1:43 AM
Okay, then you may not have the proper settings in your FreeRTOSConfig.h - Can you post it (in particular the bottom part)? It defines some hooks for FreeRTOS to use to tell touchgfx when the guitask is scheduled in and out.
I'm guessing you're using the STM32F429-DISCO application template.
/Martin
2019-07-11 1:50 AM
#ifndef FREERTOS_CONFIG_H
#define FREERTOS_CONFIG_H
/* USER CODE BEGIN Includes */
/* Section where include file can be added */
/* USER CODE END Includes */
/* Ensure stdint is only used by the compiler, and not the assembler. */
#if defined(__ICCARM__) || defined(__CC_ARM) || defined(__GNUC__)
#include <stdint.h>
extern uint32_t SystemCoreClock;
#endif
#define configUSE_PREEMPTION 1
#define configSUPPORT_STATIC_ALLOCATION 1
#define configSUPPORT_DYNAMIC_ALLOCATION 1
#define configUSE_IDLE_HOOK 1
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ ( SystemCoreClock )
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES ( 7 )
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)8192)
#define configMAX_TASK_NAME_LEN ( 16 )
#define configUSE_16_BIT_TICKS 0
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 8
#define configCHECK_FOR_STACK_OVERFLOW 2
#define configUSE_RECURSIVE_MUTEXES 1
#define configUSE_MALLOC_FAILED_HOOK 1
#define configUSE_APPLICATION_TASK_TAG 1
#define configUSE_COUNTING_SEMAPHORES 1
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 1
/* Co-routine definitions. */
#define configUSE_CO_ROUTINES 0
#define configMAX_CO_ROUTINE_PRIORITIES ( 2 )
/* Set the following definitions to 1 to include the API function, or zero
to exclude the API function. */
#define INCLUDE_vTaskPrioritySet 1
#define INCLUDE_uxTaskPriorityGet 1
#define INCLUDE_vTaskDelete 1
#define INCLUDE_vTaskCleanUpResources 0
#define INCLUDE_vTaskSuspend 1
#define INCLUDE_vTaskDelayUntil 0
#define INCLUDE_vTaskDelay 1
#define INCLUDE_xTaskGetSchedulerState 1
/* Cortex-M specific definitions. */
#ifdef __NVIC_PRIO_BITS
/* __BVIC_PRIO_BITS will be specified when CMSIS is being used. */
#define configPRIO_BITS __NVIC_PRIO_BITS
#else
#define configPRIO_BITS 4
#endif
/* The lowest interrupt priority that can be used in a call to a "set priority"
function. */
#define configLIBRARY_LOWEST_INTERRUPT_PRIORITY 15
/* The highest interrupt priority that can be used by any interrupt service
routine that makes calls to interrupt safe FreeRTOS API functions. DO NOT CALL
INTERRUPT SAFE FREERTOS API FUNCTIONS FROM ANY INTERRUPT THAT HAS A HIGHER
PRIORITY THAN THIS! (higher priorities are lower numeric values. */
#define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY 5
/* Interrupt priorities used by the kernel port layer itself. These are generic
to all Cortex-M ports, and do not rely on any particular library functions. */
#define configKERNEL_INTERRUPT_PRIORITY ( configLIBRARY_LOWEST_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )
/* !!!! configMAX_SYSCALL_INTERRUPT_PRIORITY must not be set to zero !!!!
See http://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html. */
#define configMAX_SYSCALL_INTERRUPT_PRIORITY ( configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - configPRIO_BITS) )
/* Normal assert() semantics without relying on the provision of an assert.h
header file. */
/* USER CODE BEGIN 1 */
#define configASSERT( x ) if ((x) == 0) {taskDISABLE_INTERRUPTS(); for( ;; );}
/* USER CODE END 1 */
/* Definitions that map the FreeRTOS port interrupt handlers to their CMSIS
standard names. */
#define vPortSVCHandler SVC_Handler
#define xPortPendSVHandler PendSV_Handler
/* IMPORTANT: This define is commented when used with STM32Cube firmware, when the timebase source is SysTick,
to prevent overwriting SysTick_Handler defined within STM32Cube HAL */
#define xPortSysTickHandler SysTick_Handler
/* To measure mcu load by measure time used in the dummy idle task */
#define traceTASK_SWITCHED_OUT() xTaskCallApplicationTaskHook( pxCurrentTCB, (void*)1 )
#define traceTASK_SWITCHED_IN() xTaskCallApplicationTaskHook( pxCurrentTCB, (void*)0 )
/* USER CODE BEGIN Defines */
/* Section where parameter definitions can be added (for instance, to override default ones in FreeRTOS.h) */
/* USER CODE END Defines */
#endif /* FREERTOS_CONFIG_H */I thought only configUSE_IDLE_HOOK 1, needed.
2019-07-11 1:56 AM
Okay, now show me your OSWrapper.cpp - It contains the TouchGFX Idle task hook. configUSE_IDLE_HOOK 1 is needed to call the function in touchgfx that sets up the correct task tag. If that method is missing, nothing will happen.
/Martin
2019-07-11 1:57 AM
#include <touchgfx/hal/OSWrappers.hpp>
#include "FreeRTOS.h"
#include "task.h"
#include "queue.h"
#include "semphr.h"
#include <touchgfx/hal/GPIO.hpp>
#include <touchgfx/hal/HAL.hpp>
using namespace touchgfx;
static xSemaphoreHandle frame_buffer_sem;
static xQueueHandle vsync_q = 0;
// Just a dummy value to insert in the VSYNC queue.
static uint8_t dummy = 0x5a;
void OSWrappers::initialize()
{
vSemaphoreCreateBinary(frame_buffer_sem);
// Create a queue of length 1
vsync_q = xQueueGenericCreate(1, 1, 0);
}
void OSWrappers::takeFrameBufferSemaphore()
{
xSemaphoreTake(frame_buffer_sem, portMAX_DELAY);
}
void OSWrappers::giveFrameBufferSemaphore()
{
xSemaphoreGive(frame_buffer_sem);
}
void OSWrappers::tryTakeFrameBufferSemaphore()
{
xSemaphoreTake(frame_buffer_sem, 0);
}
void OSWrappers::giveFrameBufferSemaphoreFromISR()
{
// Since this is called from an interrupt, FreeRTOS requires special handling to trigger a
// re-scheduling. May be applicable for other OSes as well.
portBASE_TYPE px = pdFALSE;
xSemaphoreGiveFromISR(frame_buffer_sem, &px);
portEND_SWITCHING_ISR(px);
}
void OSWrappers::signalVSync()
{
if (vsync_q)
{
// Since this is called from an interrupt, FreeRTOS requires special handling to trigger a
// re-scheduling. May be applicable for other OSes as well.
portBASE_TYPE px = pdFALSE;
xQueueSendFromISR(vsync_q, &dummy, &px);
portEND_SWITCHING_ISR(px);
}
}
void OSWrappers::waitForVSync()
{
// First make sure the queue is empty, by trying to remove an element with 0 timeout.
xQueueReceive(vsync_q, &dummy, 0);
// Then, wait for next VSYNC to occur.
xQueueReceive(vsync_q, &dummy, portMAX_DELAY);
}
void OSWrappers::taskDelay(uint16_t ms)
{
vTaskDelay(ms);
}
static portBASE_TYPE IdleTaskHook(void* p)
{
if ((int)p) //idle task sched out
{
touchgfx::HAL::getInstance()->setMCUActive(true);
}
else //idle task sched in
{
touchgfx::HAL::getInstance()->setMCUActive(false);
}
return pdTRUE;
}
// FreeRTOS specific handlers
extern "C"
{
void vApplicationStackOverflowHook(xTaskHandle xTask,
signed portCHAR* pcTaskName)
{
while (1);
}
void vApplicationMallocFailedHook(xTaskHandle xTask,
signed portCHAR* pcTaskName)
{
while (1);
}
void vApplicationIdleHook(void)
{
// Set task tag in order to have the "IdleTaskHook" function called when the idle task is
// switched in/out. Used solely for measuring MCU load, and can be removed if MCU load
// readout is not needed.
vTaskSetApplicationTaskTag(NULL, IdleTaskHook);
}
}
2019-07-11 2:43 AM
@Martin KJELDSEN is this file ok?
2019-07-11 2:56 AM
Okay, so actually, that looks to be correct. Hmm. When the hook calls
touchgfx::HAL::getInstance()->setMCUActive(bool);.. it will call into the MCUInstrumentation class. Do you have the option to break in there? setMCUActive() ? It's implemented in MCUInstrumentation.hpp
2019-07-11 3:13 AM
I set a breakpoint inside this function, but what should I see?
void STM32F4Instrumentation::setMCUActive(bool active)
{
if (active) //idle task sched out
{
cc_consumed += getCPUCycles() - cc_in;
}
else //idle task sched in
{
cc_in = getCPUCycles();
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.