2019-09-20 1:18 AM
I have a bunch of toggle buttons wich are on the leftmost area of the screen, but i need them to be selectable through the whole screen width. Is there any alternative of setWidth() function? because that sets width only from starting position to the right, but i need to the left (and if i put togglebutton to the left, the image will be draw in incorrect place)
2019-09-20 6:27 AM
You have the source code for buttons, so it's possible to do extend it anyway you want.
You could also "steal" the click at the view level and check if the coordinate intersects with the button along the width of the screen.
What do you think?
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.