2020-10-15 11:54 PM
we've just purchased a couple of X-NUCLEO-GFX01M1 kits and want to test them with different nucleo boards.
The X-NUCLEO board should be compatible with the following: NUCLEO-F030R8, NUCLEO-F070RB, NUCLEO-F072RB, NUCLEO-F091RC, NUCLEO-F401RE, NUCLEO-F410RB, NUCLEO-F411RE, NUCLEO-F446RE, NUCLEO-G071RB, NUCLEO-L053R8, NUCLEO-L073RZ, NUCLEO-L412RB-P, NUCLEO-L433RC-P, NUCLEO-L452RE, NUCLEO-L452RE-P and NUCLEO-L476RG.
what is the best (and quickest) way to evaluate/test the display with L4 and F4 boards?
From TouchGFX Designer there is only one choice of template available working with the STM32G0 MCUs
-DS
2020-10-23 12:39 PM
I'm in the same situation. Also, I can't find the manual for the card (UM2750). When will it be ready?
2020-12-26 7:37 AM
That's the same for me! I'm interesting to develop something with STM32 other than the "default one" they provide as a starting demo
It seems no one is taking care of that. Maybe on YouTube we can find something?
Regards
2020-12-28 1:08 AM
Touch gfx from v4.15 as a template for the xnucleo gfx board.
But where are the three demo highlighted by the teaser video :?https://youtu.be/4DSb1-yuf2c
this demo Is very impressive for a SPI screen.
thx
2020-12-28 2:22 AM
Yes, I know the video in the link you post. impressive!
The point is that I'm dealing with touchgfx by starting from a template (in my case for the STM32F746-Discovery).
Even if I'm using a template, I spent some days on YouTube to find the "adjstument" needed for running the board with proper operation of the touch screen (why that ?? Why it doesnt work buy itself without "manual" adjustment?)
But I don't want to go OT with the '746
Yes there is the template for the XNUCLEO GFX expansion board, but it refers to coupling the expansion with the STM32G071-NUCLEO or in other words the template is for the '32G017 cpu.
Is it easy to migrate form the STM32G0 to another member of the STM32 family?
I've no idea, since I never try a project starting from scratch.
Regards
Enzo
2020-12-28 4:20 AM
Hi Enzo,
Unfortunately I’ve no experience with Touch GFX. I’ve planned to acquire some and for this purpose I’ve build kind of STM32G071-NUCLEO and XNUCLEO GFX clone in order to start with a working environment and port it to other custom board with various CPU and SPI screen. That’s part of end of year vacation planning !.
To answer your question, yes it’s no so difficult to port a CubeMX HAL based software between STM32 families. Generate a project for G071- Xnucleo GFX with Touch GFX, this will be your source then generate with CubeMX a target project for your 32F746-Discovery with the same configuration (ports, names, peripheral) than the source one : open the .ioc file in source project and clone the configuration in the target, don’t forget to add ‘touchGFX’ Software pack and also ’XCUBE display extension board’ software pack. Generate the code a start porting ...
If you already made some YouTube search you should know those :
The configuration of the G071 board that should be replicated of the F746 is (this is a cubeMX report) :
Configuration STM32G071_NUCLEO
STM32CubeMX 6.1.1
Date 12/28/2020
MCU STM32G071RBTx
PERIPHERALS MODES FUNCTIONS PINS
SPI1 Transmit Only Master SPI1_MOSI PA7
SPI1 Transmit Only Master SPI1_SCK PA5
SPI2 Full-Duplex Master SPI2_MISO PC2
SPI2 Full-Duplex Master SPI2_MOSI PC3
SPI2 Full-Duplex Master SPI2_SCK PB13
Pin Nb PINs FUNCTIONs LABELs
15 PC2 SPI2_MISO
16 PC3 SPI2_MOSI
17 PA0 GPIO_EXTI0
18 PA1 GPIO_Output DISPLAY_RESET
22 PA5 SPI1_SCK
24 PA7 SPI1_MOSI
33 PB13 SPI2_SCK
48 PC8 GPIO_Input BUTTON_CENTER
49 PC9 GPIO_Input BUTTON_LEFT
57 PB3 GPIO_Output DISPLAY_DCX
59 PB5 GPIO_Output DISPLAY_CSX
63 PB9 GPIO_Output FLASH_CS
64 PC10 GPIO_Input BUTTON_DOWN
PERIPHERALS MODES FUNCTIONS PINS
SPI1 Transmit Only Master SPI1_MOSI PA7
SPI1 Transmit Only Master SPI1_SCK PA5
SPI2 Full-Duplex Master SPI2_MISO PC2
SPI2 Full-Duplex Master SPI2_MOSI PC3
SPI2 Full-Duplex Master SPI2_SCK PB13
Pin Nb PINs FUNCTIONs LABELs
1 PC11 GPIO_Input BUTTON_RIGHT
2 PC12 GPIO_Input BUTTON_UP
3 PC13 GPIO_Input BUTTON_USER
15 PC2 SPI2_MISO
16 PC3 SPI2_MOSI
17 PA0 GPIO_EXTI0
18 PA1 GPIO_Output DISPLAY_RESET
22 PA5 SPI1_SCK
24 PA7 SPI1_MOSI
33 PB13 SPI2_SCK
48 PC8 GPIO_Input BUTTON_CENTER
49 PC9 GPIO_Input BUTTON_LEFT
57 PB3 GPIO_Output DISPLAY_DCX
59 PB5 GPIO_Output DISPLAY_CSX
63 PB9 GPIO_Output FLASH_CS
64 PC10 GPIO_Input BUTTON_DOWN
Rgds
Chris
2021-01-04 11:13 AM
Dear Chris,
Thanks for you reply and Happy New Year!
I appreciated a lot your suggestions. I will try to put them in practice soon.
I'm still engaged in another project.
Keep in touch!
Regards
Enzo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.