2021-01-03 10:15 AM
I already tried to uninstall and reinstall but without success. The log file says the following error:
2021-01-03 19:11:01,782 [12] ERROR TouchGFXDomainModel.LoadSave.LoadSave: Der Wert darf nicht NULL sein.
Parametername: source
System.ArgumentNullException: Der Wert darf nicht NULL sein.
Parametername: source
bei System.Linq.Enumerable.Select[TSource,TResult](IEnumerable`1 source, Func`2 selector)
bei TouchGFXDomainModel.LoadSave.Serial.FromSerial.Convert(List`1 colorDepths)
bei TouchGFXDomainModel.LoadSave.Serial.FromSerial.Convert(SerialApplication a)
bei TouchGFXDomainModel.LoadSave.Serial.FromSerial.Convert(SerialModel m)
bei TouchGFXDomainModel.LoadSave.LoadSave.LoadDotTouchgfx(String filename)
bei TouchGFXDomainModel.LoadSave.LoadSave.Load(String filename)
I would be happy if someone can help me.
Happy new year to everyone.
Best regards
Bernhard
2021-01-03 10:16 AM
Sorry some information got lost.
I want to create an example for STM32F746 DISCO board (Progress Indicator Example). I use Win 10, and the latest TOUCH GFX Designer Version 4.16.
2021-01-03 11:44 AM
When you need this example work in 4.15 .
2021-01-04 12:11 AM
Thanks MM..1,
you are right. With 4.15 this example works. Well, in this case I will stay at 4.15.
Best regards
Bernhard
2021-01-04 12:11 AM
Thanks MM..1,
you are right. With 4.15 this example works. Well, in this case I will stay at 4.15.
Best regards
Bernhard
2021-01-04 4:47 AM
Hi,
Thank you for reporting this, I have created an internal ticket to fix this. I have been able to replicate this issue as well with any board or simulator.
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.