2020-05-11 9:42 AM
Hi all,
Do we can implement EEprom_Emulation with TouchGFX, because i want to save some data when i change them on screen.
i had tested EEprom_Emulation (in folder STM32Cube) with out touchGFX and it run normal, but when i testing EEprom_Emulation with TouchGFX that have some problem such as: hang touch, and data read from eeprom not same data i had save before that.
i had config EEPROM_START_ADDRESS 0x08070000 and program when i compile Flash property only have 15%, that mean it not over lap EEPROM_START_ADDRESS 0x08070000.
Do i have mistake in my program, or how we can tackle EEprom_Emulation with TouchGFX,
Thanks and best regards.
2020-05-11 10:22 AM
Pretty sure 0x08070000 doesn't fit on a 128KB or 256KB flash sector boundary
You might be better served making a hole lower in memory where you can use the smaller/faster sectors (32KB), and frankly implement journalled management of the flash directly rather than obfuscated through an opaque layer
2020-05-11 6:51 PM
Hi clive1.
Thank for your response.
That means I should use Eeprom have lower address, but I think if I use eeprom address 0x8010000, when I compile my program( address for start program 0x8000000), it maybe will overlap my eeprom.
Do you have any document or experience in this field, could you sharing with me more detail.
Thanks and best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.