2019-08-28 8:41 AM
Hello,
i have 25 MHz HSE Clock.
The DSI PLL settings are as follows: IDF 5, NDIV 80, ODF2
With these settings i measure an DSI clock of 100 MHz on the DSI_CKP pin.
But Cube says that the DSI clock is 200 MHz.
I use a STM32F769NI device with 2 DSI data lanes.
Do you have any idea?
BR
Daniel
2019-08-28 9:08 AM
They do on the surface look like appropriate numbers for a 200 MHz pixel clock.
As I recall the DSI clocks on both edges, effectively doubling the bandwidth, ie 100 MHz clock on pin equates to 200 Mbps on the wire.
I built a decoder for the LTDC/DSI clocks, will have to dig that up.
2019-08-28 10:28 PM
Hi Clive,
thank you for your response!
I know DSI uses double data rate (DDR) and therefore data is transfered on the rising and the falling clock edge. This means when I have a DSI clock frequency of 200 MHz I have a bandwitdth of 400 Mbit/sec.
But I don't understand why the measured DSI clock frequency is only the half of the calculated DSI clock frequency.
2019-08-29 12:13 AM
The STM32's unit clocks at 200 MHz internally so it can generate data on both edges of the 100 MHz clock on the wire.
2019-08-29 12:45 AM
void plldecode(void) // sourcer32@gmail.com
{
uint32_t vcoinput, vco;
uint32_t oscsource;
uint32_t pllcfgr = RCC->PLLCFGR;
uint32_t plli2scfgr = RCC->PLLI2SCFGR;
uint32_t pllsaicfgr = RCC->PLLSAICFGR;
uint32_t pllp, pllq, pllr;
uint32_t p, q, r;
/* Configure the PLLSAI division factor */
/* PLLSAI_VCO Input = PLL_SOURCE/PLLM */
if((pllcfgr & RCC_PLLCFGR_PLLSRC) == RCC_PLLSOURCE_HSI)
oscsource = HSI_VALUE; /* In Case the PLL Source is HSI (Internal Clock) */
else
oscsource = HSE_VALUE; /* In Case the PLL Source is HSE (External Clock) */
vcoinput = (oscsource / (uint32_t)(pllcfgr & RCC_PLLCFGR_PLLM));
vco = (vcoinput * ((pllcfgr & RCC_PLLCFGR_PLLN) >> 6));
pllp = (((pllcfgr & RCC_PLLCFGR_PLLP) >> 16) + 1) * 2;
if (pllp) p = vco / pllp; else p = 0;
pllq = (pllcfgr & RCC_PLLCFGR_PLLQ) >> 24;
if (pllq) q = vco / pllq; else q = 0;
pllr = (pllcfgr & RCC_PLLCFGR_PLLR) >> 28;
if (pllr) r = vco / pllr; else r = 0;
printf("PLL P:%9d Q:%9d R:%9d\n", p, q, r);
vco = (vcoinput * ((plli2scfgr & RCC_PLLI2SCFGR_PLLI2SN) >> 6));
pllp = (((plli2scfgr & RCC_PLLI2SCFGR_PLLI2SP) >> 16) + 1) * 2;
if (pllp) p = vco / pllp; else p = 0;
pllq = (plli2scfgr & RCC_PLLI2SCFGR_PLLI2SQ) >> 24;
if (pllq) q = vco / pllq; else q = 0;
pllr = (plli2scfgr & RCC_PLLI2SCFGR_PLLI2SR) >> 28;
if (pllr) r = vco / pllr; else r = 0;
printf("PLLI2S P:%9d Q:%9d R:%9d\n", p, q, r);
vco = (vcoinput * ((pllsaicfgr & RCC_PLLSAICFGR_PLLSAIN) >> 6));
pllp = (((pllsaicfgr & RCC_PLLSAICFGR_PLLSAIP) >> 16) + 1) * 2;
if (pllp) p = vco / pllp; else p = 0;
pllq = (pllsaicfgr & RCC_PLLSAICFGR_PLLSAIQ) >> 24; // 2..15
if (pllq) q = vco / pllq; else q = 0;
pllr = (pllsaicfgr & RCC_PLLSAICFGR_PLLSAIR) >> 28; // 2..7
if (pllr) r = vco / pllr; else r = 0;
printf("PLLSAI P:%9d Q:%9d R:%9d\n", p, q, r);
{
uint32_t dckcfgr1 = RCC->DCKCFGR1;
uint32_t divr = 2 << ((dckcfgr1 & RCC_DCKCFGR1_PLLSAIDIVR) >> 16); // 2,4,8,16
uint32_t lcdclk = r / divr;
printf("LCDCLK %9d, %6.2lf MHz\n", lcdclk, (double)lcdclk*1e-6);
}
{
uint32_t dsiwrpcr = DSI->WRPCR;
if (dsiwrpcr & 1) // Enabled
{
uint32_t odf = 1 << ((dsiwrpcr >> 16) & 0x0F); // 1,2,4,8
uint32_t idf = ((dsiwrpcr >> 11) & 0x07);
uint32_t ndir = ((dsiwrpcr >> 2) & 0x7F); // 10..124
uint32_t dsi = (HSE_VALUE * ndir) / (idf * odf);
printf("DSIPLL %9d, %6.2lf MHz\n", dsi, (double)dsi*1e-6);
printf("lbClk %9.3lf KHz\n", (double)dsi / 8000.0);
printf("TXEscape %lf\n", (double)dsi / (8000.0 * 15620.0));
}
}
}
2019-09-02 10:20 PM
Hi Clive,
many thanks for your help!
BR
Daniel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.