2019-08-30 1:45 AM
Hello
i'm trying to port the code shown in the webinar:
https://www.youtube.com/watch?v=jQO7zhX0e0Q
to the STM32H750 disco board, because i need urgently to be able to pilot a GPIO on that board.
The webinar shows the TouchGFX project genarated code, in particular on 29:54 the main.cpp is shown, which have hw_init() and touchgfx_init() functions, but in my main.cpp those functions are not there. is this because at the moment the touchGFX can't generate a CUBEMX project? any way to do that?
i also tryed to generate a project starting from CUBEMX, sinche this H750eval board is present, but when i choose that board, only the MCU is shown, not the board, so i can't configure any GPIO/Led ecc on board.
Thanks for any help
2019-09-02 1:28 AM
Hi @Zui,
CubeMX does not support TouchGFX on H7, yet. We have an H750 disco application template available through the designer, though.
You're right in that the calls to
hw_init();
touchgfx_init();are in main.cpp, but the definitions are usually in BoardConfiguration.cpp.
Try starting from TouchGFX Designer instead and make changes to GPIOs by hand - Or, do it in CubeMX in a seperate project and port those changes over to the TouchGFX project.
/Martin
2019-09-02 4:58 AM
I'm doing as you suggest, but now i can't make it work when compiled via IAR.
i started a new TouchGFX project, imported my GUI, compiled and downloaded to my board, all worked fine, but if i try do load on board same code compiled by IAR won't work (and i'm using STM32 Link Utility to flash into board)
any advice?
Tnx
2019-09-02 5:01 AM
You'll have to be more specific, i think. Can you debug your way through the application?
/Martin
2019-09-02 5:04 AM
no, i'm just using IAR for compiling, then flashing with stm32 link
2019-09-02 5:05 AM
You should be able to program using st-link and then debug the code running from internal flash using IAR.
/Martin
2019-09-02 5:08 AM
Yes i can do that (just tryedd), but how that is going to help me understan why same code, compiled with touchGFX gcc works, and compiled with IAR don't?
Thanks
2019-09-02 6:35 AM
It will help you understand where things go wrong, and then maybe, based on that, we can figure out the answer to your original question.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.