2019-11-12 2:25 AM
#define CAMERA_FRAME_BUFFER 0xC0260000
#define CONVERTED_FRAME_BUFFER 0xC0390000
I have seen a example application in the downloaded Bundle from the ST Site.
Applications/Camera Example:
In this application CAMERA is initialised with CAMERA_FRAME_BUFFER and when Capture the frame with capture command the data is retrieved from CONVERTED_FRAME_BUFFER.
I just want to know the logic behind this.
Logically the data should be available on CAMERA_FRAME_BUFFER, but why the application is retrieving from CONVERTED_FRAME_BUFFER ?
2019-11-12 3:11 AM
Got the answer, this was filled with LCD buffer and then getting the image from the CONVERTED_FRAM_BUFFER
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.