STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Proposal: Excel file alternative

Do you have any plans to rework text resources so that excel file would not longer be needed?The problem is that excel file cannot be binary compared.I bet all Git users will agree with me.Also, current excel file generator creates file, that MS Exce...

KMili by Associate III
  • 3019 Views
  • 8 replies
  • 0 kudos

Resolved! How can I do scrolling text?

Hi,I want to do a scrolling text. I think, I can use "scrollable container". But how can I scroll automatically don't know.  Is there any example about this type of usage for scrollable container? 

DCMI Memory for a camera in STM32F756

#define CAMERA_FRAME_BUFFER     0xC0260000#define CONVERTED_FRAME_BUFFER 0xC0390000I have seen a example application in the downloaded Bundle from the ST Site. Applications/Camera Example: In this application CAMERA is initialised with CAMERA_FRAME_B...

Kishore1 by Associate II
  • 1029 Views
  • 1 replies
  • 0 kudos

Behind FreeRTOS and TouchGFX Interaction

I try to debug a problem with the touch, but I cannot see how FreeRTOS does periodically the functions. See pictures from the call stack. In code the HAL methods are all virtual and I can’t find the code where they are called. It seems there is somet...

0690X00000ArjkAQAR.png
Andi by Associate III
  • 3084 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.