2021-07-30 4:21 PM
Hello,
I am studying the STM32412G-DISCOVERY and I can't explain why, in line 153 of the file /Drivers/BSP/STM32412G-Discovery/stm32412g_discovery_lcd.h (https://github.com/STMicroelectronics/STM32CubeF4), it says that the LCD_TE_PIN is GPIO_PIN_3. In the documentation (pages 26 and in the schematics), it always says that LCD_TE is PG4. As far as I understand, this pin is not really used in the code, but I find it confusing.
Thank you in advance for your reply.
[And by the way, do you know why the directory for this board is STM32412G-Discovery and not STM32F412G-Discovery (with the F)? The other boards have all the "F" (STM32F401-Discovery, STM32F429I-Discovery, ...]
Best regards,
-- Jacques
2021-07-30 8:12 PM
I see what you mean, I think the PG3 is a miss-read of the schematic, and it is PG4
Surely you can confirm the actual wiring/connectivity, and observe the periodicity of the TE signal, via looking at the PG3 and PG4 as visible within the STM32
2021-07-31 12:47 AM
Thank you very much for your reply. I will make some experiments to confirm that the signal is really on PG4. If so, should I make a pull request to the git repository?
2021-07-31 2:30 AM
That might be the most effective way to get the issue in front of someone.
2021-08-06 3:40 AM
It seems like the LCD_TE was on PG3 in the first design, and changed to PG4. But the lcd.h file has not been updated since...
A ticket has been entered.
2021-08-06 4:10 AM
Internal ticket number: 111673 (PS: This is an internal tracking number and is not accessible or usable by customers)
Chahinez.
2021-08-06 4:29 AM
Thank you very much. I am pleased to be able to contribute to the quality of the software in this way.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.