STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Touchgfx wildcard with letter d not printed

HelloI have encountered a strange problem. Actually I wanted to show a value in minutes human readable on the display (x days, y hours, z min). The value is then inserted on the display in a textarea with a wildcard. And it seems that this field has ...

JSalz.1 by Associate II
  • 2404 Views
  • 3 replies
  • 0 kudos

getClientFrameBuffer()generated data error

HiI had a probelm when I ported the programI use FSMC(8080) ,and I reffered to the stm32f412-discovoery exampleEverything else is nomal except the getClientFrameBuffer()'s bufferthis is my UI in the designer:so if the data which will load to the Gram...

0693W00000D1nRtQAJ.png 0693W00000D1nS8QAJ.png
F1412.1 by Associate
  • 891 Views
  • 0 replies
  • 0 kudos

Can TouchGFX be used with GPL code?

Hi,In the TouchGFX license it states that:"No use, reproduction or redistribution of this software package partially or totally may be done in any manner that would subject this software package to any Open Source Terms (as defined below)."Does this ...

jeremyh by Associate II
  • 1039 Views
  • 0 replies
  • 0 kudos

Correct pin for LCD_TE_PIN on STM32412G-DISCOVERY. Is it GPIO_PIN_3 (as in stm32cube source code) or GPIO_PIN_4 (as in datasheet)

Hello,I am studying the STM32412G-DISCOVERY and I can't explain why, in line 153 of the file /Drivers/BSP/STM32412G-Discovery/stm32412g_discovery_lcd.h (https://github.com/STMicroelectronics/STM32CubeF4), it says that the LCD_TE_PIN is GPIO_PIN_3. In...

JSupc.1 by Associate II
  • 3752 Views
  • 6 replies
  • 0 kudos

DSI Host on Custom Board (STM32F469 chipset)

We are currently developing a product that involves the DSI host interface. We were successful with the STM32F469 disco but we aren't having any luck with a custom solution. We are using the same series chip for our custom board as the discovery kit....

CPhip.1 by Associate II
  • 4891 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.