2020-08-04 9:58 AM
I know this seems like a simple question, but for whatever reason this is what is giving the most issues today.
Here is what I am working with:
Unicode::UnicodeChar keyboardBuffer[7][3];
Unicode::UnicodeChar* buff = keyboard.getBuffer();
Unicode:: strncpy(keyboardBuffer[keyboardSelection], buff, 3);
I am copying the keyboard buffer into keyboardBuffer[keyboardSelection].
But I need to convert this character array into an int so I can use it to properly set the time in my device and also check if the int is within range.
I have google searched and have tried several different methods but each one returns an error. I am assuming I am doing something wrong and that is why I am here asking for suggestions.
I am also using the stm32CubeIDE and do not believe it is using C++ version 11 as I am unable to use atoi.
I have also tried stringstream with this:
std::stringstream str(keyboardBuffer[keyboardSelection]);
to no avail.
help would be appreciated as I am sure I am just missing something simple.
Thank you in advanced.
EDIT:
It turns out I was simply using atoi wrong.
I have now done this:
Unicode::atoi(buff);
Unicode::snprintf(hourTextBuffer, 10, "%02d", buff);
hourText.invalidate();
but the number displayed is not correct.
EDIT2:
Problem Solved!
It ended up being very easy.
Unicode::snprintf(hourTextBuffer, 10, "%02d", Unicode::atoi(buff));
hourText.invalidate();
2020-08-04 10:38 AM
You are missing a very simple thing - the description of particular errors!
2020-08-04 11:30 AM
I didnt see the need since I would assume if it was possible to convert UnicodeChar* to an integer then it would be explained to me.
When I use keyboardBuffer[keyboardSelection] in any atoi or stringstream format I am greeted with
conversion from x to x requested
failed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.