2025-10-22 5:29 AM
I have a multi-language graphics project which requires the use of characters beyond the standard ASCII set. I have not found a working method to convert C++ wstring to TouchGFX::Unicode. I have attempted the following:
Unicode::strncpy(txtTitleBuffer, headerText.c_str(), buf_size1); //No matching funtions...
Unicode::strncpy(txtTitleBuffer, headerText, buf_size1); //No matching funtions...
Unicode::snprintf(txtTitleBuffer, buf_size1, "%s", headerText.c_str()); //Compiles without error but only shows 1st character.
Unicode::snprintf(txtPasswordTitleBuffer, buf_size1, "%s", headerText); //Compiles without error but only shows ??? which is the default undefined font character.
If possible I would like to stay with the standard C++ type for the strings and convert as it is about to be displayed as manipulating TouchGFX::Unicode is a bit clunky.
Solved! Go to Solution.
2025-10-22 7:45 AM
Hi, this works with C++20.
std::wstring ws = L"Hello";
std::u16string ws_to_u16s ( const std::wstring & ws )
{
// wchar_t is 16-bit, so direct copy works.
return std::u16string ( ws.begin (), ws.end () );
}
Unicode::snprintf ( txtTitleBuffer, buf_size1, "%s", ws_to_u16s ( ws ).data () );
2025-10-22 6:03 AM
I don't know about TouchGFX, but I assume it is related to standard C++.
Assuming you want to have a byte string which is UTF-8 encoded and TouchGFX::Unicode is such a thing:
Then it depends on your C++ version unfortunately. Up to C++ 17 at least this would be the way: https://en.cppreference.com/w/cpp/locale/codecvt.html
But it is deprecated starting with C++ 20 (though it might work probably). Then you could search for ICU (u_strToUTF8/u_strFromUTF8) - which I never used.
2025-10-22 7:45 AM
Hi, this works with C++20.
std::wstring ws = L"Hello";
std::u16string ws_to_u16s ( const std::wstring & ws )
{
// wchar_t is 16-bit, so direct copy works.
return std::u16string ( ws.begin (), ws.end () );
}
Unicode::snprintf ( txtTitleBuffer, buf_size1, "%s", ws_to_u16s ( ws ).data () );
2025-10-22 7:53 AM
And this works as well, on Windows, so no need for conversion it seems ?
std::wstring ws = L"Hello";
Unicode::snprintf ( txtTitleBuffer, buf_size1, "%s", ws.data () );
2025-10-22 8:01 AM
And so does this
constexpr std::wstring ws = L"Hello";
Unicode::snprintf ( txtTitleBuffer, buf_size1, "%s", ws.c_str () );
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.